MYZEL Lifecycle Platform Päivitykset

Tervetuloa päivityssivullemme!

Täällä tiedotamme säännöllisesti MYZEL Lifecycle Platformin uusista toiminnoista, virhekorjauksista ja optimoinneista.

Pysy ajan tasalla ja tutustu siihen, miten parannamme sovellustamme jatkuvasti suorituskyvyn, vakauden ja käyttäjäystävällisyyden parantamiseksi.

MYZEL Lifecycle Platform Päivitykset
Date Product Feature Description of change
28.07.2026 myCore
Task management Tasks for expiring/expired digital artefacts can now be created in the expired artifacts view.
Task management Tasks can be searched by keyword (ID, name, related asset,…).
Task management Tasks can now be filtered by status, creator and assignee.
Date Product Feature Description of change
07.07.2026 myCore
Task management Users can add comments to tasks to provide further context.
Task management All related tasks can be found at users and assets pages to see what tasks are open on the selected Asset.
Task management Emails are sent to assignees on task assignment to make the user aware of a new task.
Task management Users can unsubscribe/subscribe to task related emails at the preferences menu which is accessible at the user's icon.
Date Product Feature Description of change
16.06.2026 myCore
Task management Tasks can be created, edited and deleted.
Task management Upcoming and overdue tasks are visually highlighted.
Task management Task status, priority and assignee can be managed.
Task management Open points of a validation can be converted to a task.
Task management Navigate directly from a task to the associated asset or requirement within a validation.
Date Product Feature Description of change
05.05.2026 myCore
Asset management Ability to restrict which users can see which branches of the asset tree on the top nodes.
Artifact management Maximum file size which can be uploaded is increased from 100 MB to 1 GB.
Compliance management Expired artefacts now visible as a filter on the expiring artefacts widget.
mySafeDesign Risk assessment Ability to select risk status "Further Review", "Acceptable", "Not Acceptable", "Recommendation" at each risk.
myAccessControl Export asset Transfer asset to another company account includes asset groups.
Date Product Feature Description of change
14.04.2026 myCore
Time zone support Standard local user timezone used in all reports.
EU Data Act support Users are able to export all their data in machine readable format for transfer to another system (including documentation)
Languages Support for 8 new languages (Dutch, Portuguese, Korean, Swedish, Danish, Finnish, Czech, Turkish)
Date Product Feature Description of change
24.03.2026 myCore
Asset management Search for assets in the asset tree.
Artifact management Drag and drop artifacts directly onto the tab "Digital artifacts" in the asset details.
mySafeDesign Risk assessment Origin and consequences fields are replaced with values from the ISO 12100.
Copy and paste risk assessments.
Option to display a flat list of risks in the priority list.
Include PMA date on each risk.
Validate assets Transfer asset to another company account includes closed risk assessments.
Transfer asset to another company account includes closed validations.
Date Product Feature Description of change
03.03.2026 myCore
Artifact management Artifact table state is persisted as user navigates users and assets.
User management
Various updates to account activation, password reset and MFA based on feedback.
Manage compliance Production manager and MYZEL admin can also add, edit and delete artifact types when configuring compliance rules.
mySafeDesign Risk assessment When reusing a risk, duplicates are no longer displayed for selection in the reuse dialogue.
Various updates to the report based on feedback.
Transfer asset to another company account includes ongoing risk assessments.
Validate assets Transfer asset to another company account includes ongoing validations.
Date Product Feature Description of change
10.02.2026 myCore
Asset management Production manager and MYZEL admin can add, edit and delete artifact types (for now only on artifact upload and when editing an artifact).
User management A production manager needs to be located above each user in the user tree unless the user itself is an production manager or MYZEL admin. The user is warned in case this is not fulfilled.
User management Import of users from JSON file extended to support user hierarchy.
mySafeDesign Risk assessment Bulk upload of up to 100 images at a time using drag & drop.
Risk assessment Upgrade to the latest AI model. This will provide more risks identified, more detailed description of the risks and standards referenced.
Date Product Feature Description of change
20.01.2026 myCore
Asset management Additional attributes added to components of type "Interlock"
User management Search for users in the user tree
User management Update to icons in the user tree
Date Product Feature Description of change
16.12.2025 myCore User management Digital artefacts assigned to a user are only visible to the responsible production manager and the MLP administrator
User management Organisational nodes can be added to the user tree
Digital Artifacts Generated reports can now be deleted if the signed of assessment/validation has already been deleted
mySafeDesign
Risk assessment AI assisted suggestions of risks and risk mitigations based on images
Risk assessment Ability to add a caption to images used in a risk
Risk assessment Improved navigation by a step item navigation bar at the top of the risk page
Date Product Feature Description of change
02.12.2025 myCore Digital artifacts Artifact types are now available on the artifact table (no need to go into details screen)
Digital artifacts Show preview of the content of an artifact (PDF)
User management Hierarchical view (tree) of users instead of table
User management Organise and restructure the user tree using drag&drop
Language support Polish language added to MLP
Asset management 4 new valve component types available
mySafeDesign

 
Risk assessment Hotspots (help) to describe the basic functionality
Risk assessment Dragable side panels. Left and right panel can be resized up to 30 %
Risk assessment Increase risk title field so that full field is visible
Risk assessment Signed off risk assessments can be deleted
Risk assessment New button on risk reductions tab to reuse risk reductions
Date Product Feature Description of change
11.11.2025 myCore Unicode character support Unicode characters supported on all user details and PDF reports
Digital artifacts Bulk upload of documents
Digital artifacts  Show preview of the content of an artifact (images and text files)
MLP updates Link to MLP updates on Pilz.com added to help menue.
mySafeDesign
Risk assessment Add risk reduction measure on risk reduction tab
Risk assessment Able to assign/unassign a risk from a risk reduction measure
Risk assessment Able to delete a risk reduction measure from the risk reduction tab
Risk assessment Able to edit machine details from within a risk assessment
myAccessControl Compliance rules in I.A.M. Enforce new user defined compliance rules in I.A.M.
Date Product Task Change
21.10.2025 myCore Rules Builder  Compliance overview on machines in assets view.
Rules Builder  Compliance overview on user in users view.
Rules Builder  Horizontal widgets mode (compact view) in the compliance dashboard.
Rules Builder  Icon added to compliance widgets to easily distinguich user rules from machine rules.
Rules Builder  Layout improvements
Bulk Asset Import Schema, Sample & readme available to download from import screen.
PTM Import Import of users from a .ptm file and link to transponders.
PTM Import Import of groups from a .ptm file.
Asset Mgmt When creating the asset you can now add a picture
mySafeDesign Risk assessment Able to delete a group (section)
Risk assessment Post measure assessment report
Risk assessment Include motivation field in report
Risk assessment Markup & crop support on touch devices
Risk assessment Display all risk reduction measures in risk reductions tab
Risk assessment Create an assessment from the context menu
myAccessControl I.A.M Enforce new compliance rules

 

Top
Yhteystiedot

Pilz Skandinavien K/S, sivuliike Suomessa
Elannontie 5
01510 Vantaa
Finland

Puhelin: +358 10 3224030
Sähköposti: [email protected]

Inside Sales



Puhelin: +358 10 3224030
Sähköposti: [email protected]

Tekninen tuki

Puhelin: +358 10 3224030 / +45 74436332
Sähköposti: [email protected]

Avaa yhteyslomake
Puhelin:+358 10 3224030
Sähköposti: [email protected]

Miten voimme auttaa?


Olen tietoinen siitä, että kerättyjä henkilötietoja käytetään ilman suostumustani ainoastaan sopimuksen käsittelyyn ja tiedustelujeni käsittelyyn. Lisätietoja tietosuojasta ja tietosuojavastaavamme yhteystiedot löydät täältä: Pilz-tietosuoja
Suostumuksen peruuttaminen on mahdollista milloin tahansa (sähköposti riittää).

* Pakollinen kenttä