17 dec. 2021

Pilz hardware not affected by "Log4Shell" vulnerability in software library Log4j Vulnerability is highly unlikely to be exploited in Pilz Software products

Dear Madam or Sir,

On December 10th, 2021, the BSI (the German Federal Office for Information Security) published a cyber security alert on the so-called "Log4Shell" vulnerability in the software library Log4j. Log4j is used in many Java applications.

From the BSI alert:

"An IT security vendor blog [LUN2021] reports on vulnerability CVE-2021-44228 [MIT2021] in log4j versions 2.0 through 2.14.1, which may allow attackers to execute their own program code on the target system and thus compromise the server."

https://www.bsi.bund.de/SharedDocs/Cybersicherheitswarnungen/DE/2021/2021-549177-1032.pdf

Further information is available at:

https://www.bsi.bund.de/DE/Themen/Unternehmen-und-Organisationen/Informationen-und-Empfehlungen/Empfehlungen-nach-Angriffszielen/Webanwendungen/log4j/log4j_node.html

https://www.cisa.gov/uscert/apache-log4j-vulnerability-guidance (in English)

Pilz's analysis revealed the following:

  • Pilz hardware components do not use Java and thus no log4j. Therefore, these components are not affected.
  • Pilz Software products partially use log4j versions 2.0 to 2.14.1 (current vulnerability CVE-2021-44228). Analyses to date have shown that it is highly unlikely that the vulnerability can be exploitedIf, contrary to expectations, there is a risk, we will publish a security advisory.

  • In some Pilz Software products, log4j version 1.2.x is used. The exploitation of the vulnerability in this version (CVE 2021-4104) requires, among other things, a specific configuration. However, this configuration is not used in Pilz Software products.

We hope this information is helpful to you. If you have any further questions, please contact our technical support: [email protected].

With best regards

Pilz GmbH & Co. KG

Top
hoofdkantoor

Pilz Belgium CV
Poortakkerstraat 37/0201
9051 Sint-Denijs-Westrem
België

Telefoon: +32 (0)9 321 75 70
E-mail: [email protected]

Was dit artikel nuttig?
Open het contactformulier
Telefoon:+32 (0)9 321 75 70
E-mail: [email protected]

Wat kunnen we voor u doen?


Het is mij bekend dat de verzamelde persoonsgegevens zonder mijn toestemming uitsluitend worden gebruikt voor het uitvoeren van het contract en het behandelen van mijn verzoeken. Meer informatie over de gegevensbescherming alsmede de contactgegevens van onze functionaris voor gegevensbescherming vindt u hier: Pilz gegevensbescherming
De toestemming kan te allen tijde worden ingetrokken (e-mail is voldoende).

* Verplicht veld