19 Nov 2015

PNOZmulti Configurator - Version 10 now available

Version 10.0.0 of the PNOZmulti Configurator is now available. Discover the highlights of the latest version.

Version 10.0.0 of the PNOZmulti Configurator is now available. The configuration tool is ingeniously simple and simply ingenious; you can use it to configure all control systems PNOZmulti. Here are some of the highlights of Version 10:
 

  • It supports the new base unit PNOZ m B1 from the control system PNOZmulti 2. PNOZ m B1 has a lot to offer: for the first time, there are no inputs and outputs on the base unit. The system is adapted to the application by selecting expansion modules. As a user, you only pay for what you actually need. Much larger projects are possible with PNOZ m B1, with up to 1024 connection lines. It is also now possible to set the data and time for PNOZ m B1 in the PNOZmulti Configurator.
     
  • Version 2.0 supports the motion monitoring modules from the control system PNOZmulti 2 and are the first expansion modules to allow the configuration of special module programs (mIQ), which are executed directly on the module. Time-critical subprocesses can be run directly in the module, reducing reaction times significantly. Should the base unit switch to a safe state, the module can independently undertake a fast shutdown or soft shutdown. This guarantees maximum flexibility within the application


You can download the demo software from our download area (for registered users).

Purchasing a licence converts the demo software to a full version. Please note: a new software licence is required from each new version, any existing licence will no longer be valid.


Further information:

Download of PNOZmulti Configurator

Readme for Software PNOZmulti Configurator 10.0.0

PNOZmulti Configurator - Video tutorials

Configurable control systems PNOZmulti 2

 

PNOZmulti Configurator version 10.0.0 – hardware configuration with the new PNOZ m B1 base unit