Functional safety

What does functional safety mean?

Labyrinth of standards

The causes of hazards and therefore the technical measures applied to avoid them can vary widely. As a result, different types of safety are differentiated, by the cause of potential hazards for example.

“Functional safety” is the term used when safety depends on the correct function of a control system.

Risk assessment plays a central role with regard to functional safety requirements. The steps you need to consider when assessing and reducing risk on machinery come from the standard EN ISO 12100. The evaluation and verification of safety functions are the prevail of the standards EN ISO 13849 and EN IEC 62061, provided the required safeguarding is dependent on a control system. The safety integrity requirements (PL, SIL) are derived from the risk estimation.

Quo vadis "functional safety"?

Two arrows leading to standards

In automation too, there is a trend towards digitisation. The rising level of complexity means that configurable or programmable control systems are increasingly used to safeguard plant and machinery. When designing machine control systems, this question often arises in the course of the risk assessment: how do you select the required safety level for safety-related control functions? Manufacturers must select and then combine the components in accordance with certain criteria. The risk estimation looks at the probability of a component failing to danger. The probabilities of failure of the various components must then be examined together. The required safety level is determined via graphs, which illustrate the severity of injury and the frequency or duration of exposure. The greater the risk, the higher the controller's safety-related requirements. Every safety function is examined in the process. For example, protection against unintended restart or shutting down via the E-STOP function in the case of danger, or even ensuring that the machine is still safe, should the controller fail. 

Productivity must also be considered alongside demands for a safe machine. If not, the incentive to tamper with safety devices will increase.  

The requirements of safety-related parts of machine control systems are defined in both ISO 13849 and IEC 62061.

Revision of the standards ISO 13849 and IEC 62061

Both standards had to be updated to continue to represent the "state of the art". The latest edition of IEC 62061 was published on 22 March 2021. ISO 13849 has reached FDIS status; that means that the content can no longer be changed. The impetus to revise both standards stemmed not just from the routine revision and upgrade to the state of the art, but also from the many discussions that took place during the failed attempt to unify the two standards within IEC ISO 17305. 

The following changes affect both ISO 13849 and IEC 62061:  

  • Changed methodology for defining the required safety level (PL or SIL) 
  • Changed requirements of the application software, depending on the complexity and the selected programming languages 
  • Allow subsystems that were developed in accordance with one standard to be used in the other 
Changes ISO 13849 - 2023 Changes IEC 62061 - 2021 
  • Overview (Clause 4) 
  • Definition of safety functions (Clause 5) 
  • Software (Clause 7) 
  • Validation (Clause 10 was adopted from EN ISO 13849-2) 
  • Combinations of subsystems (Annex H) 
  • EMC requirements (Annex L) 
  • Typical safety requirements (Annex M) 
  • Software requirements (Use cases, Annex N) 
  • Scope: independent of technology (no longer limited to E/E/PES) 
  • New annexes for failure rates (Annex C), diagnostic coverage (Annex E) and reliability calculations (Annex K) 
  • “SIL CL” renamed “SIL” 
  • New SW level for application software (Clause 8) 
  • Degrees of independence with SW verification and general validation 
  • EMC requirements (Clause 6.6) 
  • SW-based parameter setting clarified (Clause 6.7) 
  • Added requirements for periodic test, e.g. proof test 
  • Security 
Compass pointing to ISO 13849

Transition periods and harmonisation

ISO 13849-1 was published in 2023; this was followed in May 2024 by publication of EN ISO 13849-1:2023 in the EU Official Journal. It comes into force with a transition period until 15.05.2027, and replaces the previous standard EN ISO 13849-1:2015. Harmonisation refers to the currently valid Machinery Directive 2006/42/EC, which will be replaced on 20 January 2027 by the Machinery Regulation (EU) 2023/1230. It can be assumed that EN ISO 13849-1:2023 will be harmonised, with some straightforward adjustments to the Machinery Regulation (EU) 2023/1230. Harmonisation of EN ISO 13849-1:2015 to the Machinery Regulation (EU) 2023/1230 is not planned as yet. For this reason we recommend that EN ISO 13849-1:2023 is applied as soon as possible.

In March 2024, IEC 62061:2021/AMD1:2024 was published with some amendments and additions to IEC 62061:2021. EN IEC 62061:2021/A1:2024 was published in July 2024. A further revision of IEC 62061:2021 was published in March 2026 and June 2026 respectively with IEC 62061:2021/AMD2:2026 and EN IEC 62061:2021/A2:2026.

As soon as an international IEC or ISO standard is published as an EU standard in the Official Journal of the European Union, presumption of conformity applies. That means that a manufacturer who abides by the specifications of the standard can assume that they comply with the health and safety requirements of the Machinery Directive and so, as part of the conformity assessment with the declaration of conformity, can affix the CE mark to their machine. The ratified, international standards can be applied as soon as they have been published on the IEC and ISO websites. However, it is advisable to deal with the expected development at an early stage.

Standard Status
IEC 62061:2021
  • Published (2021-03)
EN IEC 62061:2021
  • Published (2022-01)
Harmonised to the MD 2006/42/EC (2022-04)
ISO 13849-1:2023
  • Published (2023-04)
EN ISO 13849-1:2023
  • Published (2023-11)
Harmonised to the MD 2006/42/EC (2024-05)
IEC 62061:2021/AMD1:2024
  • Published (2024-03)
EN IEC 62061:2021/A1:2024
  • Published (2024-07)
IEC 62061:2021/AMD2:2026
  • Published (2026-03)
EN IEC 62061:2021/A2:2026
  • Published (2026-06)
ISO 13849-2:20xx In progress
EN ISO 13849-2:20xx In progress

 

Functional safety at a glance

A man with laptop standing in an office.

The aim of functional safety is always to protect humans and machines from hazards. In Europe, the relevant functional safety standards in the engineering sector are listed in the Machinery Directive. Download our "Functional safety" poster now and discover at a glance the procedure for risk assessment and risk reduction in accordance with EN ISO 12100. You can draw on two important standards, derived from this A standard: EN ISO 13849-1 or EN IEC 62061.

Further information

Overview
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
Telephone:+49 711 3409 444
Mail: [email protected]

What can we do for you?


I understand that, unless I give my consent, any personal data collected will only be used for processing orders and dealing with my enquiries. Further information on data protection and contact details for our data protection officer are available here: Pilz data protection
Consent can be withdrawn at any time (E-Mail will suffice).

* Mandatory field