Here you'll find answers relating to machinery safety, industrial safety regulations, directives and standards. Or take advantage of the specialist knowledge of our experts by asking them your specific question.
FAQ: Laws and standards
Are you looking for answers relating to machinery safety?
Overview of FAQ: Laws and standards
Category
Reset filter
- When the emergency stop is operated on a machine, does it have to be reset/acknowledged on each individual machine?
- What has changed with the standard EN ISO 12100?
- What colour must an area stop pushbutton be?
- Is it possible to connect as many emergency stop pushbuttons as possible in series, in order to simplify a circuit (designed to Cat. 4)?
- What do we mean by an assembly of machinery?
- When do we speak of a "competent person"?
- When is a conveyor line considered no longer accessible?
- What is the difference between Type A, B and C standards?
- Is there a standard that states how high the reduced speed may be, on conveyors for example, if the conveyor is not enclosed?
- Can single and dual-channel emergency stops be used together on a plant?
- Must an operating mode selector switch be safely evaluated?
Top
Headoffice
Pilz GmbH & Co. KG
Felix-Wankel-Straße 2
73760 Ostfildern
Germany
Telephone: +49 711 3409-0
E-Mail: [email protected]
Technical Support
Telephone: +49 711 3409 444
E-Mail: [email protected]
Americas
- Brazil: + 55 11 4942-7032
- United States (toll-free): +1 877-PILZUSA (745-9872)
- Mexico: +52 55 5572 1300
- Canada: +1 888-315-PILZ (315-7459)
Europe
- Italy: +39 0362 1826711
- United Kingdom: +44 1536 460866
- Spain: +34 938497433
- Sweden: +46 300 13990 / +45 74436332
- France (toll-free): +33 3 88104000
- Turkey: +90 216 577 55 52
- Denmark: +45 74436332
- Germany: +49 711 3409 444
- Austria: +43 1 7986263-444
- Belgium: +32 9 321 75 70
- Russia: +7 495 6654993
- Portugal: +351 229 407 594
- Ireland: +353 21 4804983
- Finland: +358 10 3224030 / +45 74436332
- Switzerland: +41 62 889 79 32
- Netherlands: +31 347 320477
Asia Pacific
- Singapore: +65 6829 2920
- New Zealand: +64 9 6345350
- Japan: +81 45 471 2281
- Australia (toll-free): +61 3 9560 0621 / 1300 723 334
- Taiwan: +886 70 1015 0068 (ç¶å°ç¶²è·¯é»è©±)
- South Korea: +82 31 778 3390
- Thailand: +66 210 54613
- China: +86 400-088-3566
Was this article helpful?