Industrial Security is versatile and comes into play on several levels. In OT and production, the principle of Industrial Security primarily serves to protect machinery from hazards caused by human action. This principle protects machinery from hazards such as cyber attacks or manipulation.
Industrial Security to reduce risk
Industrial Security risk assessment
The first thing to do when examining production for Industrial Security is to carry out a risk assessment. This reveals the dangers and risks that a machine is exposed to from “cyberspace” and the measures that must be taken to minimise them.
The security risk assessment should always be carried out in the following steps:
- Identify assets: What do I want to protect?
- Analyse threats: What are the risks on the asset I want to protect?
- Determine relevant protection objectives: What objectives do I want to achieve?
- Analyse and assess risks: How likely is it that a risk will occur?
- Analyse threat vectors
- Create and implement security concept
- Review the implementation
- Regular re-assessments
- Select and implement protective measures: How can I protect against potential risk?
- Resilience management: What to do after an attack? How can I anchor the idea of security more firmly in the company?
Excursus: Security Level
Security levels define the level of security that plant operators or manufacturers wish to achieve using security measures. The relevant information is provided by a prior risk assessment. This defines what is to be protected and determines the probability of this asset being attacked. The Security level (SL) is selected accordingly. These days, SL-2, i.e. protection against “intentional violation using simple means with low resources, generic skills and low motivation” should be seen as the minimum standard. To keep this minimum standard, the company needs a specific security maturity level. The best firewall is useless if a company’s employees continue to write their passwords on post-it notes and stick them on their PC screens, or if they do not run updates. The more the company is involved in security as an issue, the higher the overall protection will be. Therefore an overall security concept is important.
The Security levels at a glance:
- Security level 1: Protection against casual or coincidental violation
- Security level 2: Protection against intentional violation using simple means
- Security level 3: Protection against intentional violation using sophisticated means
- Security level 4: Protection against intentional violation using sophisticated means and extensive resources
Six tips for enhanced Industrial Security measures
A detailed security risk assessment is essential in order to protect a machine in a targeted and specific manner But generic measures can also increase security. Any measure is better than none. The following strategies help you implement security in your company:
1. Defence in depth:
This principle is based on always placing new and different obstacles in the path of intruders. That makes it more difficult for attackers to achieve their objective. The point is to create as many obstacles as possible on as many levels as possible, as each individual measure can of course be defeated. An important part of this concept is to always take the human factor into account.
2. Organisational measures:
It is important that all of a company’s employees internalise Security. It is advisable to set up guidelines that apply to your own employees as well as partners such as suppliers and service providers. Since trust is good but control is better, anyone responsible for security should check compliance with these guidelines and support them if necessary.
3. Training:
Not everybody is an IT expert, so your employees require regular Security training. Pilz seminars are held at their headquarters in Ostfildern near Stuttgart, on the customer's premises or as a web seminar, and are aimed at plant and machine designers, but also at operators.
4. Segmentation based on the “zones and conduits” principle:
Devices with similar security requirements are grouped into shared zones and separated from each other by firewalls or secure routers. The connections between these zones (“conduits”) are precisely controlled so that only authorised devices and defined communication interfaces can send and receive data. As a result, it is possible to set up a separate zone for safety systems, for example, and to safeguard it with particularly stringent protective measures, without disrupting normal plant operations unnecessarily.
5. Firewalls:
Although routers and switches can support security mechanisms, you should also employ industrial firewalls in your control network. This helps to protect the control technology on plant and machinery from the manipulation of process data, for example.
6. Patch management:
Patches are particularly necessary when you become aware of security-related vulnerabilities in the software. This concerns application software and embedded software. You should consider not only patches and updates released by the manufacturer, but also third-party software (e.g. office applications, PDF Reader). A patch process helps to define responsibilities and procedures.
Further essential requirements of Industrial Security
Where Industrial Security is concerned, if you look at IEC 62443 you will find a series of basic requirements, called “foundational requirements”, which describe in an abstract way technical methods for increasing security:
Identification and access control (IAC)
This ensures that the devices and the information they contain can only be accessed or modified by legitimate entities with the required permissions. These permissions are necessary to ensure the safe operation of the plant or installation and to guarantee the functionality of the IACS (Industrial Automation and Control System).
Usage control (UC)
Usage control (UC) ensures that only authorised entities can use the devices and/or information to carry out valid and necessary tasks, which are essential for the safety and productivity of the plant or installation. So it's a question of permissions. The principle of “least privilege” should be respected.
System integrity (SI)
This foundational requirement ensures that no unauthorised changes can be made to the data in the communication channels, so that correct data is always available. For example, the values displayed must correspond to the actual values and must not have been manipulated.
Data confidentiality (DC)
All data in a machine should remain confidential and must not be capable of being viewed by outsiders or unauthorised insiders.
Restricted data flow
This foundational requirement ensures that data only flows to areas where it is really needed. This reduces the possibility of data being viewed or manipulated without authorisation. This means that the system architecture should be designed in such a way that the system can be divided into zones and conduits with appropriate security levels. Using devices such as a unidirectional gateway or a data diode can help.
Timely response to events
It is important to ensure that the IACS provides the necessary capabilities to respond to security breaches. This includes notifying the appropriate authority, documenting evidence of the breach, and taking timely corrective action when such an incident is discovered.
Resource availability
It is necessary to ensure that the IACS is designed and operated in such a way that a situation cannot arise in which a system can no longer be controlled or, in the worst case, can no longer even be brought to a safe state. This means that the safety system must not be prevented from putting the plant into a safe state or from fulfilling its protective function, even under a denial-of-service attack.
Additional system requirements are defined for each of these foundational requirements. These can be used as a basis for the implementation of security measures, and become more extensive depending on the level of technical security you wish to achieve.
Pilz GmbH & Co. KG
Felix-Wankel-Straße 2
73760 Ostfildern
Germany
Telephone: +49 711 3409-0
E-Mail: [email protected]
Telephone: +49 711 3409 444
E-Mail: [email protected]
Americas
- Brazil: + 55 11 4942-7032
- United States (toll-free): +1 877-PILZUSA (745-9872)
- Canada: +1 888-315-PILZ (315-7459)
- Mexico: +52 55 5572 1300
Europe
- Belgium: +32 9 321 75 70
- Ireland: +353 21 4804983
- France (toll-free): +33 3 88104000
- Sweden: +46 300 13990 / +45 74436332
- Turkey: +90 216 577 55 52
- Italy: +39 0362 1826711
- Russia: +7 495 6654993
- Portugal: +351 229 407 594
- Finland: +358 10 3224030 / +45 74436332
- Netherlands: +31 347 320477
- Germany: +49 711 3409 444
- United Kingdom: +44 1536 460866
- Spain: +34 938497433
- Denmark: +45 74436332
- Switzerland: +41 62 889 79 32
- Austria: +43 1 7986263-444
Asia Pacific
- Thailand: +66 210 54613
- South Korea: +82 31 778 3390
- China: +86 400-088-3566
- Australia (toll-free): +61 3 9560 0621 / 1300 723 334
- Japan: +81 45 471 2281
- New Zealand: +64 9 6345350
- Singapore: +65 6829 2920
- Taiwan: +886 70 1015 0068 (ç¶å°ç¶²è·¯é»è©±)