Basics - harmonised standards, directives and laws in the EU

What is the relationship between standards, directives and laws?

Standards puzzle

The European Union is experiencing ever closer union. This leads to increasing harmonisation of laws, regulations and provisions in engineering. First, the EU formulates general safety objectives via directives. These safety objectives require precise specification. Specific regulation occurs via standards.

EU directives only take effect when countries within the EU incorporate them into domestic law. In each EU country, a law or provision refers to the relevant EU directive and thus elevates it to the status of domestic law.

The situation is different with regulations. An EU regulation can come into effect immediately after it has been ratified by the EU Commission, without the need for it to be incorporated into domestic law.

Standard met, requirement met – harmonised standards

Standards alone have no legal relevance. They do not achieve this until they are published in the Official Journal of the EU or through domestic laws and provisions. Publication of these harmonised standards triggers “presumption of conformity”. Users applying the standard can therefore assume that they are acting in compliance with the law and directives. The burden of proof has therefore been reversed in the event of a claim. If a harmonised standard refers to a standard that has not been harmonised, the latter can obtain a status comparable to that of harmonisation.


 

Standards, directives and laws in the EU

Harmonisation work on EU standards – consultancy firm ERNST & YOUNG confirmed as HAS contractor

Maze with files

International standardisation work is important, but without harmonisation to European directives and regulations, it is incomplete in practice and does not achieve its objective. In the worst case, differing product and safety requirements at IEC and ISO level could become CEN/CENELEC versions of standards - that's a very critical situation for commercial enterprises as global market players!

Today, standards are almost always developed and published at international IEC and ISO level. In an ideal scenario, they should be adopted unchanged into the European body of standards. In the EU, responsibility for adoption as harmonised standards lies with the European Commission. This has delegated the comparison with the essential health and safety requirements of the EU/EC directives / regulations to harmonised standards consultants (HAS Consultants). Until January 2022, approval, coordination and budget monitoring was administered by the consultancy firm ERNST & YOUNG (E&Y), acting as HAS contractor. However, the EU budget for this advisory function was spent by October 2021 and the harmonisation process stalled.

The new contract, again with E&Y as contractual partner, has now been in place since August 2022. In the meantime, harmonisation work has been more or less on ice. The result is a not inconsiderable harmonisation backlog, which must now be processed step by step, so that publication in the Official European Journal can take place as soon as possible.

The new contract contains the following important and relevant changes:

  1. HAS consultants may spend up to 25 % of their evaluation working time attending meetings and in communication within standards committees. This has the advantage of avoiding harmonisation discrepancies at an earlier stage.
  2. In future there will be a clear, structured assessment procedure for the harmonisation evaluation:
  • NO harmonisation deviations ISO/IEC and CEN/CENELEC = “COMPLIANT”
  • Critical harmonisation deviations = “LACK of COMPLIANCE” = Presumption of conformity not provided or
  • “CONDITIONAL COMPLIANCE” = Presumption of conformity with limitations

It is to be hoped that the new contract and changed operational procedure will make harmonisation work more efficient, with standards harmonised more quickly and finally published in the Official Journal of the European Union. As a result, presumption of conformity with directives and regulations would formally and finally be provided.

Procedure for publishing harmonised standards in the Official Journal of the European Union

On 18.3.2019, the EU Commission published Implementing Decision (EU) 2019/436 in the EU Official Journal, outlining the changes to the list of harmonised standards for machinery with regard to the Machinery Directive 2006/42/EC. It updated the list of standards, whose application triggers presumption of conformity in accordance with the Machinery Directive 2006/42/EC.

A complete list of harmonised standards was published in the Official Journal of the European Union until the above decision came into force. The publication was valid until the next complete catalogue was published. The last version of this catalogue, containing an overview of all the standards harmonised under the Machinery Directive, appeared on 9 March 2018.

The practice for publication has fundamentally changed.

From Implementing Decision (EU) 2019/436, a complete, consolidated list will no longer appear, only the changes from the previous document will be described.

Publications now have the following structure, with a total of 3 annexes:

  • Annex I: Newly published harmonised standards
     
  • Annex II: Harmonised standards that are published in addition to the previous publication with certain restrictions
     
  • Annex III: Previously harmonised standards, withdrawn from the Official Journal of the European Union

Since that first decision, further decisions have appeared at regular intervals, for which you must observe the procedure described above. You'll find an overview of these decisions on the EU Commission's homepage. There you'll find a summary of all the harmonised standards published in the Official Journal of the European Union. The summary includes all the standards for which there was presumption of conformity at the time the list was prepared, as well as the standards that have already been withdrawn from the Official Journal.

However, this summary has no legal force. The EU Commission provides this summary for information purposes only. Although every possible precaution has been taken to ensure that the summary is regularly updated and is correct, errors can occur and the summary may be incomplete at a certain point in time. So the user has no alternative but to watch out for the standards relevant to them in the implementing decisions.

Should you need support, Pilz offers a comprehensive range of machinery safety services.

To services

New procedure established for publishing harmonised standards in the Official Journal of the European Union

Overview

Further information:

Top
Headoffice

Pilz GmbH & Co. KG
Felix-Wankel-Straße 2
73760 Ostfildern
Germany

Telephone: +49 711 3409-0
E-Mail: [email protected]

Technical Support
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
Telephone:+49 711 3409 444
Mail: [email protected]

What can we do for you?


I understand that, unless I give my consent, any personal data collected will only be used for processing orders and dealing with my enquiries. Further information on data protection and contact details for our data protection officer are available here: Pilz data protection
Consent can be withdrawn at any time (E-Mail will suffice).

* Mandatory field