With a lockout/tagout (LoTo) system developed specially for your machinery, you will have a reliable solution, which your staff can use to safely control hazardous energy during repair and maintenance routines.
Lockout tagout system
Control hazardous energy safely: with the Pilz lockout/tagout system
Effective lockout/tagout with the Pilz lockout/tagout system
Your requirements
To provide staff with effective protection from hazardous energy sources you can introduce measures in the form of a LoTo system. These guarantee that machines and other work equipment are isolated from the energy supply, whether electrical, mechanical, hydraulic, etc. That way you can be assured that an unintended restart is excluded.
Our services
The LoTo system from Pilz comprises two stages: LoTo analysis and LoTo procedure development. As part of the LoTo analysis we examine the existing documentation, such as the plant’s LoTo policies and the procedures for preventing re-energisation. This is to ensure they meet your own internal corporate requirements. Once the LoTo analysis has been successfully completed, we develop a detailed LoTo procedure for the specific machine, in graphic form. This describes the individual requirements step by step. As a result it is guaranteed that all hazardous energies are controlled through the lockout/tagout procedure.
The Pilz LoTo services include:
- Analysis of existing plant
- Analysis of the company’s LoTo policies
- Analysis of existing procedures
- Development of new procedures
- Compliance with regulatory requirements
- Staff training on the LoTo procedure and the identification of hazardous energy
Your benefits at a glance
- Boost the productivity of your plant
- Reduce downtimes on your plant, at the same time achieving optimum safety
- You meet the various country-specific requirements or recommendations
- Implement solutions such as the American 21 CFR 1910.147 standard or the European work equipment directives 2009/104/EC and 2006/42/EC, for example. These comply with the applicable legislation.
You too can benefit from these services
Pilz GmbH & Co. KG
Felix-Wankel-Straße 2
73760 Ostfildern
Germany
Telephone: +49 711 3409-0
E-Mail: [email protected]
Telephone: +49 711 3409 444
E-Mail: [email protected]
Americas
- Canada: +1 888-315-PILZ (315-7459)
- Mexico: +52 55 5572 1300
- United States (toll-free): +1 877-PILZUSA (745-9872)
- Brazil: + 55 11 4942-7032
Europe
- France (toll-free): +33 3 88104000
- Denmark: +45 74436332
- Austria: +43 1 7986263-444
- Portugal: +351 229 407 594
- Belgium: +32 9 321 75 70
- Russia: +7 495 6654993
- Turkey: +90 216 577 55 52
- Spain: +34 938497433
- Italy: +39 0362 1826711
- Finland: +358 10 3224030 / +45 74436332
- Ireland: +353 21 4804983
- Germany: +49 711 3409 444
- Switzerland: +41 62 889 79 32
- Sweden: +46 300 13990 / +45 74436332
- Netherlands: +31 347 320477
- United Kingdom: +44 1536 460866
Asia Pacific
- South Korea: +82 31 778 3390
- Taiwan: +886 70 1015 0068 (ç¶å°ç¶²è·¯é»è©±)
- Australia (toll-free): +61 3 9560 0621 / 1300 723 334
- China: +86 400-088-3566
- Singapore: +65 6829 2920
- Japan: +81 45 471 2281
- New Zealand: +64 9 6345350
- Thailand: +66 210 54613