Interlinked machinery

Interlinked machinery

We speak of interlinked plant or machinery, for example, when machines are joined to form a complete system or when another machine is added to an existing machine.

What are the characteristics of interlinked machinery?

To assess whether it is an interlinked plant, the following questions must be answered:

  • Is there a functional connection? Do the plant sections work together as a whole and form a unit?
  • Is there a control-related connection? Are the plant sections operated as a whole?
  • Is a safety-related connection required? Do the plant sections function as a whole in terms of safety?

 

Mandatory marking for interlinked machinery

If the interlinking of several subsections can be expected to have functional, control-related and safety-related effects on the overall plant, then the conformity assessment procedure must also be carried out for the overall plant.

In this case it means that the whole process must be carried out for the relevant plant sections (examination of interfaces) in accordance with the Machinery Directive, from the risk assessment through to attaching the CE mark.

Headoffice

Pilz GmbH & Co. KG
Felix-Wankel-Straße 2
73760 Ostfildern
Germany

Telephone: +49 711 3409-0
E-Mail: pilz.gmbh@pilz.de

Technical Support

Telephone: +49 711 3409 444
E-Mail: support@pilz.com

Americas

  • Mexico: +52 55 5572 1300
  • Brazil: + 55 11 4942-7032
  • United States (toll-free): +1 877-PILZUSA (745-9872)
  • Canada: +1 888-315-PILZ (315-7459)

Europe

  • Ireland: +353 21 4804983
  • Austria: +43 1 7986263-444
  • Finland: +358 10 3224030 / +45 74436332
  • Italy: +39 0362 1826711
  • Russia: +7 495 6654993
  • Spain: +34 938497433
  • Denmark: +45 74436332
  • Switzerland: +41 62 889 79 32
  • Germany: +49 711 3409 444
  • Belgium: +32 9 321 75 70
  • Turkey: +90 216 5775552
  • Netherlands: +31 347 320477
  • France (toll-free): +33 3 88104000
  • Sweden: +46 300 13990 / +45 74436332
  • Portugal: +351 229 407 594
  • United Kingdom: +44 1536 460866

Asia Pacific

  • South Korea: +82 31 778 3390
  • New Zealand: +64 9 6345350
  • Japan: +81 45 471 2281
  • Taiwan: +886 2 25700068
  • Singapore: +65 6829 2920
  • Thailand: +66 210 54613
  • China: +86 400-088-3566
  • Australia (toll-free): +61 3 9560 0621 / 1300 723 334
Was this article helpful?