The modular safety gate system from Pilz now includes the PSENmlock handle module. As a comprehensive solution, the gate module has an integrated actuator as well as an integrated escape release. In conjunction with the safety gate sensor PSENmlock for safe interlocking and safe guard locking, the handle module represents a safe, individually adaptable solution for accessible gates.
Ostfildern, Mar 18, 2021
PSENmlock handle module expands the modular safety gate system from Pilz - Gates safely in hand
Safe guard locking is enabled by the two-channel control on the guard locking device. As such, the switch is particularly suitable for use on machines with a hazardous overrun, which also require safe guard locking up to the highest category performance level e.
Safety combined with high flexibility
The PSENmlock handle module can be used for both left and right-hinged gates. It can be fitted on the inside or outside and is compatible for both swing gates and sliding gates. Due to these different options, the gate module can be used for various gates. So users benefit from maximum flexibility during installation.
Danger zone under control
On the outside of the secured gate is the yellow handle, through which the actuator is disengaged for closing or opening. An escape release can only be triggered via the red handle in the inside. As a result, people can leave a danger zone potentially emerging inside the machinery space at any time. The PSENmlock handle module has a lockout bar for up to 5 locks. This prevents the machine from restarting unintentionally following a stop. This increases safety on accessible gates and so avoids accidents.
Modular, adaptable safety on gates
The PSENmlock handle module is the latest addition to the Pilz modular safety gate system. As a modular safety gate solution with access control, the safety gate system provides sensors, escape release, handles, a diagnostic system and a pushbutton unit with optional integrated access permission system as well as an appropriate evaluation device. Users benefit from rapid assembly and installation. All modules in the safety gate system can be assembled individually, providing flexible safeguarding for accessible gates. Combined with the configurable safe small controller PNOZmulti 2 from Pilz, the result is a safe complete solution for safety gate monitoring.
Further information on the modular safety gate system
and PSENmlock handle module from Pilz.
Pilz GmbH & Co. KG
Felix-Wankel-Straße 2
73760 Ostfildern
Germany
Telephone: +49 711 3409-0
E-Mail: pilz.gmbh@pilz.de
Telephone: +49 711 3409 - 158
E-Mail: publicrelations@pilz.com
Americas
- Mexico: +52 55 5572 1300
- Brazil: + 55 11 4942-7032
- United States (toll-free): +1 877-PILZUSA (745-9872)
- Canada: +1 888-315-PILZ (315-7459)
Europe
- Ireland: +353 21 4804983
- Austria: +43 1 7986263-444
- Finland: +358 10 3224030 / +45 74436332
- Italy: +39 0362 1826711
- Russia: +7 495 6654993
- Spain: +34 938497433
- Denmark: +45 74436332
- Switzerland: +41 62 889 79 32
- Germany: +49 711 3409 444
- Belgium: +32 9 321 75 70
- Turkey: +90 216 5775552
- Netherlands: +31 347 320477
- France (toll-free): +33 3 88104000
- Sweden: +46 300 13990 / +45 74436332
- Portugal: +351 229 407 594
- United Kingdom: +44 1536 460866
Asia Pacific
- South Korea: +82 31 778 3390
- New Zealand: +64 9 6345350
- Japan: +81 45 471 2281
- Taiwan: +886 2 25700068
- Singapore: +65 6829 2920
- Thailand: +66 210 54613
- China: +86 400-088-3566
- Australia (toll-free): +61 3 9560 0621 / 1300 723 334