Ostfildern, Apr 6, 2021

New module for bending angle measurement on the camera-based protection system PSENvip 2 from Pilz - Making bending processes more productive!

A new module for bending angle measurement is now available for the camera-based protection system PSENvip 2 from Pilz, which forwards usable image data to the press controller. So the operator sees the bending angle value directly on the user interface (HMI) when press braking, removing the need for expensive angle measurement systems and complex manual measurements. So the time and costs involved in the initial and subsequent adjustment of the system are reduced to a minimum. The bending process can be implemented productively and safely with PSENvip 2, thereby guaranteeing high availability on press brakes.

Over and above the time and cost savings, users also save space that would otherwise be needed to install additional devices.

Innovative technology even for rugged applications
The camera-based protection system PSENvip 2 from Pilz monitors the whole bending process using innovative optics. When installed on the upper die of the press brake, the PSENvip 2 detects even the smallest foreign body in the protected field between the transmitter and receiver, enabling productive work practices in complete safety. Instead of a laser light source, PSENvip 2 uses an LED-based solution, in which simple illumination of the receiver along the upper tool is sufficient. Even under rugged application conditions, with vibration, reflection and external or diffused light for example, the protection system guarantees very high availability.

All-round package for safe press braking
The camera-based protection system PSENvip 2 offers maximum safety for press brakes as a complete solution with the Fast Control Unit in the automation system PSS 4000 in accordance with EN ISO 12622. The complete solution guarantees faster processing, so a shorter overrun distance and therefore an even faster shutdown of the bending processes. Maximum productivity and simple handling make for an efficient bending process.

You can find more information about PSENvip here

A new module for bending angle measurement is now available for the camera-based protection system PSENvip 2 from Pilz, which forwards usable image data to the press controller. (Photo: Pilz GmbH & Co. KG)
A new module for bending angle measurement is now available for the camera-based protection system PSENvip 2 from Pilz, which forwards usable image data to the press controller. (Photo: Pilz GmbH & Co. KG)

A new module for bending angle measurement is now available for the camera-based protection system PSENvip 2 from Pilz, which forwards usable image data to the press controller. (Photo: Pilz GmbH & Co. KG)

Headoffice

Pilz GmbH & Co. KG
Felix-Wankel-Straße 2
73760 Ostfildern
Germany

Telephone: +49 711 3409-0
E-Mail: pilz.gmbh@pilz.de

Corporate and Technical Press

Telephone: +49 711 3409 - 158
E-Mail: publicrelations@pilz.com

Americas

  • Mexico: +52 55 5572 1300
  • Brazil: + 55 11 4942-7032
  • United States (toll-free): +1 877-PILZUSA (745-9872)
  • Canada: +1 888-315-PILZ (315-7459)

Europe

  • Ireland: +353 21 4804983
  • Austria: +43 1 7986263-444
  • Finland: +358 10 3224030 / +45 74436332
  • Italy: +39 0362 1826711
  • Russia: +7 495 6654993
  • Spain: +34 938497433
  • Denmark: +45 74436332
  • Switzerland: +41 62 889 79 32
  • Germany: +49 711 3409 444
  • Belgium: +32 9 321 75 70
  • Turkey: +90 216 5775552
  • Netherlands: +31 347 320477
  • France (toll-free): +33 3 88104000
  • Sweden: +46 300 13990 / +45 74436332
  • Portugal: +351 229 407 594
  • United Kingdom: +44 1536 460866

Asia Pacific

  • South Korea: +82 31 778 3390
  • New Zealand: +64 9 6345350
  • Japan: +81 45 471 2281
  • Taiwan: +886 2 25700068
  • Singapore: +65 6829 2920
  • Thailand: +66 210 54613
  • China: +86 400-088-3566
  • Australia (toll-free): +61 3 9560 0621 / 1300 723 334