Press pack FACHPACK 2022

Content

Press releases

  • Pilz at FACHPACK 2022, Hall 3c, Stand 223 - Safe, secure and flexible packaging!
  • Pilz offers TÜV-SÜD-certified solution for safe monitoring of cardboard feed in the packaging sector - safeguard cardboard feed efficiently

Additional content

Background information:

  • Safe, secure and flexible: Automation solutions for the entire packaging industry - Sustainable packaging
  • In addition to safety, key aspects for guards are efficiency, economy and digitisation - Safety gate management 4.0
  • PSENradar, PSENscan and PSENopt II: Safe radar systems and optoelectronic sensor technology for greater productivity - All-round protection for stationary and mobile applications
  • Modular diagnostic solutions for the factory of the future - Smart diagnostics any time, any place
  • Company profile

Customer references/success stories:

  • Sema Systemtechnik: This tray former is only open for efficiency
  • Mosburger GmbH: Production's rolling!
  • Poco Loco: Greater efficiency for the tortilla chip production line
  • ACMI S.p.A.: Avoiding risks during bottle filling
  • Wächter packaging machines: Clever folding with PSENslock and PNOZmulti 2
  • EuroChem: Danger clearly identified!

Press releases

Additional content

Photographic material

Modules for access permission are integrated into modern safety gate systems to ensure that only authorised persons gain access to the application, i.e. safety gate monitoring and access control are combined, with industrial security included. As an example, the modular safety gate system from Pilz is operated via the pushbutton unit PITgatebox (centre): It is available in various pre-configured versions with combinations of pushbuttons, key switches and E-STOP pushbuttons. (Photo: © Pilz GmbH & Co.KG)

If maximum safety is to be combined with unconditional economy, then non-contact magnetic safety switches PSENmag come into the frame, as they can also be concealed and can monitor the position of the guard as well as covering general position monitoring. (Photo: © Pilz GmbH & Co.KG)

When production processes require intervention, light curtains provide optimum protection for plant and machinery. The PSENopt range from Pilz provides finger, hand and body protection, depending on the requirement. In production as well as logistics, it is always the first choice whenever the process or production requires continuous infeed and outfeed, an absence of barriers or exchange between human and machine as part of HRC applications. (Photo: © Pilz GmbH & Co.KG)

Comprehensive protection for industrial automation networks: The firewall SecurityBridge from Pilz also guarantees that data communication with any other network subscribers outside of the Pilz product range is monitored. (Photo: © Pilz GmbH & Co.KG)

The modular safety gate system from Pilz combines sensors, escape release and handles, as well as control and pushbutton units: Within the system, the PSENmlock handle module has an integrated actuator as well as an integrated escape release. Combined with the safety gate sensor PSENmlock for safe interlocking and safe guard locking, the result is an individually adaptable solution for accessible gates. (Photo: © Pilz GmbH & Co.KG)

Together with the configurable small controller PNOZmulti 2, the safe radar system PSENradar represents a safe, complete, radar-based solution for monitoring protection zones – including conformity assessment. It is particularly appropriate when areas and zones are to be safeguarded on shop floors with a high incidence of dust and dirt, such as when packaging bulk materials for example. (Photo: © Pilz GmbH & Co.KG)

Additional photographic material

Top
Head office

Pilz Australia Safe Automation
Unit 1, 12-14 Miles Street

Australia

Telephone: +61 3 9560 0621 / 1300 723 334
E-Mail: [email protected]

Press Center

Telephone: +61 3 9560 0621
E-Mail: [email protected]

Open contact form
Telephone:+61 3 9560 0621
Mail: [email protected]

What can we do for you?


I understand that, unless I give my consent, any personal data collected will only be used for processing orders and dealing with my enquiries. Further information on data protection and contact details for our data protection officer are available here: Pilz data protection
Consent can be withdrawn at any time (E-Mail will suffice).

* Mandatory field