As soon as a communication module is connected, the device automatically switches over to this interface on start-up. However, it is possible to switch back to USB via the display.
Small controllers
Configurable control systems PNOZmulti 2
Which interface is preferred when a communication module is connected to the base unit PNOZ m B0?
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
Was this article helpful?