Controllers

PLC controllers and I/O systems

What is the essential difference between the control system PSSuniversal PLC and PSSuniversal multi in the automation system PSS 4000?

The control system PSSuniversal multi is a trimmed-down version of the control system PSSuniversal PLC. PSSuniversal multi does not offer the following features, whereas the PSSuniversal PLC does:

  • Only programming/configuration via the editor PASmulti is possible, no programming in accordance with EN/IEC 61131-3
  • No non-volatile variables
  • No standard resource
  • Maximum of 5 SafetyNET p subscribers can be connected
  • No Profinet
  • No Ethernet/IP