Join our live webcast on August 25th at 2pm to learn how the Pilz Safety Gate System PSENsgate helps you to protect your process and employees in one convenient package, delivers protection up to PLe, SIL3, and how you can easily add it to your CAD drawings using our available EPLAN macros.
21 août 2020
Maximizing worker safety in body-entry applications

Automated processes introduce unique safety challenges that require actively monitored protection for the machine operator, the machine itself, and the product that is being produced. This often requires machines to be fenced-in with access being provided via lockable doors, but a lockable door can also present its own hazard, as it introduces the risk that an operator can get trapped in the danger zone which can result in serious injury if the process is restarted before they have exited from the guarded area. Additionally, automated processes need to be shut down in an orderly manner to protect the machine and the product that it is producing, and doors must remain locked until confirmation is received that all machinery has been returned to a safe condition before access can be permitted.
Join our live webcast on August 25th at 2pm to learn how the Pilz Safety Gate System PSENsgate solves these challenges in one convenient package, delivers protection up to PLe, SIL3, and how you can easily add it to your CAD drawings using our available EPLAN macros.
Pilz Automation Safety Canada L.P.
6695 Millcreek Drive, Unit 8
Mississauga, ON, L5N 5R8
Canada
Téléphone: +1 905 821 7459
E-mail: info@pilz.ca