Here you'll find answers relating to machinery safety, industrial safety regulations, directives and standards. Or take advantage of the specialist knowledge of our experts by asking them your specific question.
FAQ: Laws and standards
Are you looking for answers relating to machinery safety?
Overview of FAQ: Laws and standards
Category
Reset filter
- When the emergency stop is operated on a machine, does it have to be reset/acknowledged on each individual machine?
- What has changed with the standard EN ISO 12100?
- What colour must an area stop pushbutton be?
- Is it possible to connect as many emergency stop pushbuttons as possible in series, in order to simplify a circuit (designed to Cat. 4)?
- What do we mean by an assembly of machinery?
- When do we speak of a "competent person"?
- When is a conveyor line considered no longer accessible?
- What is the difference between Type A, B and C standards?
- Is there a standard that states how high the reduced speed may be, on conveyors for example, if the conveyor is not enclosed?
- Can single and dual-channel emergency stops be used together on a plant?
- Must an operating mode selector switch be safely evaluated?
Top
Pilz Österreich
Pilz Ges.m.b.H. Sichere Automation
Wagramer Straße 19
1220 Wien
Österreich
Telephone: +43 1 7986263-0
E-Mail: [email protected]
Technischer Support
Telephone: +43 1 7986263-444
E-Mail: [email protected]
Was this article helpful?