Is it possible to connect as many emergency stop pushbuttons as possible in series, in order to simplify a circuit (designed to Cat. 4)?

In a Category 4 architecture, a series connection of emergency stop pushbuttons is allowed because the emergency stop is only a secondary safeguard.

It is assumed that the emergency stop will only be operated in hazardous situations - and even then only one emergency stop pushbutton will be operated.
As part of the risk assessment in accordance with the industrial safety regulations, the operator must establish the intervals in which the safety functions must be inspected and the format that inspection will take.

Where is the limit in this case?
The limit lies in the required performance level. This is because the series connection of multiple safety components worsens the overall result. If you can reach the required PL by connecting the emergency stop pushbuttons in series, then the number is not inappropriate.

Is every switch rated as an SRP/CS in the context of the standard EN ISO 13849?
In the safety assessment you can connect all emergency stop switches in series, i.e. you only need to create one SRP/CS. However, as described above, the series connection may worsen the PL and so it may be possible to create several SRP/CS.

 

Top
Pilz Österreich

Pilz Ges.m.b.H. Sichere Automation
Wagramer Straße 19
1220 Wien
Österreich

Telephone: +43 1 7986263-0
E-Mail: [email protected]

Technischer Support

Telephone: +43 1 7986263-444
E-Mail: [email protected]

Was this article helpful?
Open contact form
Telephone:+43 1 7986263-444
Mail: [email protected]

What can we do for you?


I understand that, unless I give my consent, any personal data collected will only be used for processing orders and dealing with my enquiries. Further information on data protection and contact details for our data protection officer are available here: Pilz data protection
Consent can be withdrawn at any time (E-Mail will suffice).

* Mandatory field