Is there a standard that states how high the reduced speed may be, on conveyors for example, if the conveyor is not enclosed?

Safe reduced speed and continuous flow conveyors

The C standard EN 619:2002 for continuous handling equipment and systems only states speed for cases in which people may travel on the conveyor. These are:

Continuous flow conveyors on which persons may travel:

  • Floor level: Conveying speed of 0.3 m/s
  • 0.3 m above floor level: Conveying speed of 0.15 m/s
  • Full railings: Conveying speed of 0.5 m/s

VDI 2854 also deals with the issue of safe, reduced speed. This states that a speed is deemed to be safe if the person has time to escape from a hazardous event.

 

Top
Pilz Österreich

Pilz Ges.m.b.H. Sichere Automation
Wagramer Straße 19
1220 Wien
Österreich

Telephone: +43 1 7986263-0
E-Mail: [email protected]

Technischer Support

Telephone: +43 1 7986263-444
E-Mail: [email protected]

Was this article helpful?
Open contact form
Telephone:+43 1 7986263-444
Mail: [email protected]

What can we do for you?


I understand that, unless I give my consent, any personal data collected will only be used for processing orders and dealing with my enquiries. Further information on data protection and contact details for our data protection officer are available here: Pilz data protection
Consent can be withdrawn at any time (E-Mail will suffice).

* Mandatory field