Закрыть
Pilz International
Пожалуйста, выберите страну
Выберите свою страну, чтобы получить доступ к предназначенным для нее материалам
Вы искали «PMC SI6A062 terminal set (Y/Z)»
User licence for the PSS WIN-PRO software for use of the full version
on an additional workstation. Includes a licence key for activating
the full functionality. Only valid for expanding a basic licence. Note:
Does not include software! CD must be ordered separately, if required.
по запросу
Basic licence for the PSS WIN-PRO software for use of the full version
on one workstation. Includes a licence key for activating the full
functionality. Note: Does not include software! CD must be ordered
separately, if required.
по запросу
Multi-User licence for the PSS WIN-PRO software for for use of the
full version on several workstations. Includes a licence key for
activating the full functionality. Note: Does not include software! CD
must be ordered separately, if required.
по запросу
User licence for the PSS WIN-PRO software for use of the service
version on an additional workstation. Includes a licence key for
activating the full service functionality. Only valid for expanding a
basic licence. Note: Does not include software! CD must be ordered
separately, if required.
по запросу
Upgrade licence for updating the version number of an existing project
licence for the service version of the PSS WIN-PRO software. Includes
a licence key for activating the service functionality. Note: Does not
include software! CD must be ordered separately, if required.
по запросу
Basic licence for the PSS WIN-PRO software for use of the service
version on one workstation. Includes a licence key for activating the
service functionality. Note: Does not include software! CD must be
ordered separately, if required.
по запросу
Temporary licence for the software PSS WIN-PRO for use of the service
version on a workstation. Includes a licence key for activating the
service functionality for a period of two months Note: Does not
include software! CD must be ordered separately, if required.
по запросу
Temporary licence for the software PSS WIN-PRO for use of the service
version on a workstation. Includes a licence key for activating the
service functionality for a period of four months Note: Does not
include software! CD must be ordered separately, if required.
по запросу
Upgrade licence for updating the version number of an existing basic
licence for the service version of the PSS WIN-PRO software. Includes
a licence key for activating the service functionality. Note: Does not
include software! CD must be ordered separately, if required.
по запросу
Temporary licence for the software PSS WIN-PRO for use of the service
version on a workstation. Includes a licence key for activating the
service functionality for a period of three months Note: Does not
include software! CD must be ordered separately, if required.
по запросу
Multi-User licence for the PSS WIN-PRO software for using the service
version on several workstations. Includes a licence key for activating
the service functionality. Note: Does not include software! CD must be
ordered separately, if required.
по запросу
Upgrade licence for updating the version number of an existing
Multi-User licence for the service version of the PSS WIN-PRO software.
Includes a licence key for activating the service functionality. Note:
Does not include software! CD must be ordered separately, if required.
по запросу
Upgrade licence for updating the version number of an existing user
licence for the service version of the PSS WIN-PRO software. Includes
a licence key for activating the service functionality. Note: Does not
include software! CD must be ordered separately, if required.
по запросу
PSSu, электронный модуль, отказоустойчивый, цифровые входы и выходы, 1вход,
1 выход тестовых импульсов на 0,25 A, 1 выход, 2 А, двухполюсный, защитаот короткого замыкания, защита от перегрузки,
обратная связь в свободной форме, для повышенных требований к окружающейсреде.
по запросу
PSSu, электронный модуль, отказоустойчивый, цифровые входы и выходы, 4выхода,
0,5 A, однополюсный, положительное переключение, защита от короткогозамыкания, защита от перегрузки,
обратная связь в свободной форме, для повышенных требований к окружающейсреде.
по запросу
PSSu, электронный модуль, отказоустойчивый, аналоговые входы и выходы, 1вход,0
- 25,59 мА, двухполюсный, дифференциальный вход, разрешение 12 бит, дляповышенных
требований к окружающей среде.
по запросу
PSSu, электронный модуль, отказоустойчивый, аналоговые входы и выходы, 1вход,-
- 10,24 - 10,23 В, двухполюсный, дифференциальный вход, разрешение 13бит, для повышенных
требований к окружающей среде.
по запросу
PSSu, электронный модуль, отказоустойчивый, цифровые входы и выходы, 4входа,
2 выхода тестовых импульсов 0,25 A, для повышенных требований кокружающей среде.
по запросу
PSSu, электронный модуль, отказоустойчивый, цифровые входы и выходы, 2выхода,
2 A, однополюсный, положительное переключение, защита от короткогозамыкания, защита от перегрузки,
обратная связь в свободной форме, для повышенных требований к окружающейсреде.
по запросу
PSSu, электронный модуль, отказоустойчивый, цифровые входы и выходы, 2выхода,
контакты реле, 8 A, Н/З, беспотенциальный, для повышенных
требований к окружающей среде.
по запросу
Следующие продукты были добавлены в Вашу Корзину
Сохранить корзину
Создать новый заказ или оформить индивидуальное ценовое предложение.