Interlinked machinery

Interlinked machinery

We speak of interlinked plant or machinery, for example, when machines are joined to form a complete system or when another machine is added to an existing machine.

What are the characteristics of interlinked machinery?

To assess whether it is an interlinked plant, the following questions must be answered:

  • Is there a functional connection? Do the plant sections work together as a whole and form a unit?
  • Is there a control-related connection? Are the plant sections operated as a whole?
  • Is a safety-related connection required? Do the plant sections function as a whole in terms of safety?

 

Mandatory marking for interlinked machinery

If the interlinking of several subsections can be expected to have functional, control-related and safety-related effects on the overall plant, then the conformity assessment procedure must also be carried out for the overall plant.

In this case it means that the whole process must be carried out for the relevant plant sections (examination of interfaces) in accordance with the Machinery Directive, from the risk assessment through to attaching the CE mark.

Top
Pilz Österreich

Pilz Ges.m.b.H. Sichere Automation
Wagramer Straße 19
1220 Wien
Österreich

Telephone: +43 1 7986263-0
E-Mail: [email protected]

Technischer Support

Telephone: +43 1 7986263-444
E-Mail: [email protected]

Was this article helpful?
Open contact form
Telephone:+43 1 7986263-444
Mail: [email protected]

What can we do for you?


I understand that, unless I give my consent, any personal data collected will only be used for processing orders and dealing with my enquiries. Further information on data protection and contact details for our data protection officer are available here: Pilz data protection
Consent can be withdrawn at any time (E-Mail will suffice).

* Mandatory field