EMC Directive

EMC Directive

When networking of plants is increasing and the use of electrical devices in the machine environment is on the rise, EMC - a directive todetermine the electromagnetic emission of devices continues to be of great importance. Electrical devices can disrupt the function of other devices or plants, but that's not all. If electromagnetic emission is not controlled, such devices can also present a considerable safety risk for man and machine.

That's why the EMC Directive regulates the electromagnetic compatibility (EMC) of all devices that are put into service or placed on the market.

The EMC Directive can be found on the homepage of the European Commission.

Official title of the EMC Directive

DIRECTIVE 2014/30/EU OF THE EUROPEAN PARLIAMENT AND OF THE COUNCIL of 26 February 2014 on the harmonisation of the laws of the Member States relating to electromagnetic compatibility (recast).

Related standards

EN 50370-1/-2
EN 61000 series
EN 61326

Top
Pilz Österreich

Pilz Ges.m.b.H. Sichere Automation
Wagramer Straße 19
1220 Wien
Österreich

Telephone: +43 1 7986263-0
E-Mail: [email protected]

Technischer Support

Telephone: +43 1 7986263-444
E-Mail: [email protected]

Was this article helpful?
Open contact form
Telephone:+43 1 7986263-444
Mail: [email protected]

What can we do for you?


I understand that, unless I give my consent, any personal data collected will only be used for processing orders and dealing with my enquiries. Further information on data protection and contact details for our data protection officer are available here: Pilz data protection
Consent can be withdrawn at any time (E-Mail will suffice).

* Mandatory field