Minimum distances between the danger zone and safeguard are specified in order to avoid hazards to persons. These are used to avoid crushing parts of the human body.
Effectiveness of safeguards through minimum distances
The minimum distances consist of two components:
- The walking / hand speed multiplied by the system reaction time and
- An additional value, which depends on the height of the danger zone and the height of the safeguard. This additional value may be up to 1 200 mm.
Standard for minimum distances on machinery
Standard | Title |
---|---|
EN ISO 13854 | Safety of machinery Minimum distances - to avoid crushing of parts of the human body |
Pilz Österreich
Pilz Ges.m.b.H. Sichere Automation
Modecenterstraße 14
1030 Wien
Österreich
Telephone: +43 1 7986263-0
E-Mail: pilz@pilz.at
Technischer Support
Telephone: +43 1 7986263-444
E-Mail: techsupport@pilz.at
Was this article helpful?