Fixed guards

Fixed guards

A fixed guard is part of a machine that guarantees protection by means of a physical barrier. The guard may consist of a safety fence, barrier, covers or similar. It may be welded, glued or attached using fixing systems (bolts, rivets etc.). Fixed guards make it more difficult to access the machine physically.

Regulations for fixed guards

In accordance with the provisions of the Machinery Directive, fixed guards must be fixed by systems that can be opened or removed only with tools. Their fixing systems must remain attached to the guards or to the machinery when the guards are removed. Where possible, guards must be incapable of remaining in place without their fixings.

 

Alternatives to safeguards

If guards are neither possible nor sensible, control technology solutions are used. Should a person approach a danger source, these will shut the machine down or bring the machine to a safe state by other means. All that remains is indicative safety technology: In this case, the residual dangers are indicated in the operating manual or on the machine itself.

 

Standards for fixed guards

Standard Title
EN ISO 14120

Safety of machinery
Guards. General requirements for the design and construction of fixed and movable guards

Top
Pilz Österreich

Pilz Ges.m.b.H. Sichere Automation
Wagramer Straße 19
1220 Wien
Österreich

Telephone: +43 1 7986263-0
E-Mail: [email protected]

Technischer Support

Telephone: +43 1 7986263-444
E-Mail: [email protected]

Was this article helpful?
Open contact form
Telephone:+43 1 7986263-444
Mail: [email protected]

What can we do for you?


I understand that, unless I give my consent, any personal data collected will only be used for processing orders and dealing with my enquiries. Further information on data protection and contact details for our data protection officer are available here: Pilz data protection
Consent can be withdrawn at any time (E-Mail will suffice).

* Mandatory field