The "P" at the end of a unit description stands for "pluggable", i.e. for types with plug-in connection terminals.
There are two types: plug-in screw terminals and plug-in push-in spring-loaded terminals. The spring-loaded terminals are identified by the "C" in the unit description, e.g. PNOZ X3P C.
What does the "P" at the end of a unit description stand for, e.g. on PNOZ X3P?
Safety relays PNOZ X
Top
Pilz Österreich
Pilz Ges.m.b.H. Sichere Automation
Wagramer Straße 19
1220 Wien
Österreich
Telephone: +43 1 7986263-0
E-Mail: [email protected]
Technischer Support
Telephone: +43 1 7986263-444
E-Mail: [email protected]
Was this article helpful?