Software tool PNOZmulti Configurator – Versions and updates

All relevant information on current and previous versions of the software tool PNOZmulti Configurator.

Stay up to date with the PNOZmulti Configurator

On this page you will find the latest information, innovations and guidelines for the versions of the PNOZmulti Configurator software tool.

Find out which functions have been added and how you can achieve more efficient configuration in future.

PNOZmulti Configurator Version 11.7 - SRA parameter support for EtherCAT FSoE and cascading function on the PNOZ m C0

  • SRA parameter support for EtherCAT FSoE

This means that, in future, FSoE SubInstances that exclusively support SRA parameters can also be connected via the FSoE MainInstance PNOZmulti 2. This broadens the range of applications for safe communication and offers greater flexibility when integrating relevant devices.

The FSoE SubInstance checks the CRC of these parameter settings, thereby ensuring that the parameter values are synchronised in a way that's consistent and transparent.

Benefit to you: greater compatibility, clear security testing and a further step towards comprehensive support for modern FSoE architectures.
SRA configuration is available to support FSoE SubInstances. All previously available FSoE modules are compatible.

  • Cascading function on the base unit PNOZ m C0

The PNOZmulti standalone base unit PNOZ m C0 offers 8 safe inputs and 4 safe semiconductor outputs. What's new: In the PNOZmulti Configurator you can configure up to six safe inputs as cascading inputs. This allows machine zones to be clearly structured or modular plant and machinery to be flexibly interlinked.

If you are a user with cascaded PNOZelog devices, this new function enables an easy exchange by evaluating PNOZelog OSSD outputs at a PNOZ m C0 input.

Cascading brings tangible benefits in engineering and in operation:

  • Reduced hardware and wiring effort: fewer components and cables mean lower costs and faster implementation.
  • Scalable zone concepts: machine modules can be set up hierarchically and expanded at any time.
  • Consistent safety logic: A "global stop" is propagated in an ordered manner across all levels, right down to individual sub-zones.
Ethernet and round connectors with

Questions and answers on Version 11.7

What does CRC mean in this context?

CRC stands for Cyclic Redundancy Check and is a check sum of the entire SRA parameter set (Safety Related Application Parameter). It serves as clear evidence that several devices are operating with exactly the same safety-related parameters.

What is the SRA parameter's CRC used for?

The CRC is used to ensure that all participating devices have the same SRA status. The safe connection between the devices is established only if the CRC matches.

Which devices have an SRA parameter set?

  • The EtherCAT MainDevice (e.g. IndustrialPI)
  • The FSoE MainInstance (e.g. PNOZmulti 2)

Both devices have their own SRA parameter sets, which must be logically identical.

Does the system compare the individual SRA parameters directly?

No. The FSoE SubInstance does not compare each individual parameter, but only the CRC for the complete parameter sets. This makes it easier to compare and reduces the risk of discrepancies.

How does the CRC get from the EtherCAT MainDevice to the FSoE MainInstance? The CRC of the EtherCAT MainDevice is:

The CRC of the EtherCAT MainDevice is:

  • read and
  • manually transferred to the parameter page of the PNOZmulti Configurator.

When is the safety connection established?

The safe connection is only established if:

  • the CRC of the EtherCAT MainDevice
  • and the CRC of the FSoE MainInstance

are an exact match.

What does a matching CRC actually mean?

An identical CRC means:

  • The SRA parameter sets are identical
  • There is no discrepancy in the safety-related settings
  • The requirement for permitted and safe communication is met

What happens if the CRC does not match?

If the CRC is different:

  • The system assumes different SRA states
  • The safe connection is not established
  • Safety-related communication remains disabled

Why is this CRC comparison safety-related?

The CRC comparison stops devices with:

  • obsolete,
  • faulty or
  • unintentionally changed

safety parameters from communicating with each other. This makes it a central component of functional safety.

Safe Ethernet Connection and storage of PNOZmulti projects in the Pilz Cloud – from PNOZmulti Configurator Version 11.6

Between the automation system PSS 4000 and the base units PNOZ m B1 / PNOZ m B1 Burner of the safe small controller PNOZmulti 2, a safe data connection can be configured at bit level if both controllers are to be used in one system architecture. Using the Safe Ethernet Connection software blocks, the previously separate "worlds" can be linked safely via Ethernet. The failsafe block “FS_SafeEthernet_Connection 2” is available in the software platform PAS4000 and the block “Safe Ethernet Connection Status” is available in the PNOZmulti Configurator for this purpose. In the case of both blocks, the data that is to be exchanged is simply stored in the respective user program – no further configuration is required. Investment protection for your plant is guaranteed; no need to convert fully to a different system

Benefits to you:

  • Expand your existing plant without changing the system – PNOZmulti and PSS 4000 communicate with each other safely.
  • Protect your investment by re-using existing components.
  • Involves no additional wiring – Safe connection via software blocks
  • Safe connection between both systems is easy to configure
  • Full diagnostic capability in both systems

Another feature of Version 11.6 is the ability to save your project to the cloud on the Myzel Lifecycle Platform (MLP): all PNOZmulti 2 project data is stored centrally at the same point and can be called up there at any time. Shorter project runtimes and simple documentation of your current PNOZmulti 2 projects in the new cloud solution from Pilz.

Up to 6 devices of the electronic access permission system PITreader are supported on the base units PNOZ m B1 and PNOZ m B1 burner (previously 4) – for more flexible access permissions: from a simple enable through to a complex permission matrix with individual codings.

 

PNOZmulti 2 and PSS 4000 showing a safe Ethernet connection and data exchange

All PNOZmulti 2 base units Safe and Secure – From Version 11.5 of the software tool PNOZmulti Configurator

Application of the Machinery Regulation 2023/1230 (MR) is mandatory from 20 January 2027. One requirement of the MR states that Industrial Security is a mandatory element for the safety of machinery. To meet this requirement, security functions such as user administration and access management have been installed on the PNOZmulti 2 base units to protect the devices from unauthorised access. To access a base unit or perform changes via the PNOZmulti Configurator, a user must authenticate themself with their access data. A higher-level password policy has also been defined, which applies to the assignment of passwords when PNOZmulti projects are created. A limited number of login attempts to access a project ensures that the user account is locked for a certain period of time if consecutive login attempts fail. This protects the device and prevents manipulation.

Another innovation in the software tool concerns the safe fieldbus module PNOZ m EF EtherCAT FSoE:

If you wish to switch from the standard EtherCAT fieldbus module PNOZ m ES EtherCAT to the safe FSoE fieldbus module, the configuration you created is transferred via a migration function when you swap the device. So the conversion is user-friendly and effortless, with just a few clicks in the software tool. Using FSoE means that safe plant structures can be implemented with a “one-cable solution” at fieldbus level. As a result, machines are highly available, reliable and safe.

Your application advantages:

  • Software tool can be used free of licensing costs.
Modular small controllers PNOZmulti 2 in various sizes, extracted on a white background

Software PNOZmulti Configurator – What's new in Version 11.4

The software tool PNOZmulti Configurator is used to configure the hardware of the safe small controllers PNOZmulti 2 and to create the safety circuit. The original configurable safety program is proven to be easy to use.

Version 11.4 includes these new features:

  • Hardware:

Decentralised input and output modules of protection type IP67 with 8 safe inputs and 4 safe semiconductor outputs, which allow the direct connection of decentralised peripherals via four 5-pin M12 female connectors to PNOZmulti 2. In total up to 64 sensors or actuators can be flexibly monitored in the field. Less wiring saves costs during commissioning. A version with stainless steel screw connections is available, for use in the food industry for example.

  • A new ESI file:

Version 102, for the secure Safety over EtherCAT module PNOZ m EF EtherCAT FSoE has been integrated into the software tool. Using FSoE means you can implement safe plant structures with a “one-cable solution” at fieldbus level.

  • Motion monitoring modules:

Frequency filtering can be configured to suppress short-term implausible frequency signals or EMC interference.

  • Security functions:

The base unit PNOZ m B1 protects you against unauthorised access via user management. To access the device or perform certain tasks via PNOZmulti Configurator, a user must authenticate with their access data. Thus using PNOZmulti 2 is not only safe but also secure!

 

The software displayed on a tablet

Software PNOZmulti Configurator – What’s new in Version 11.3

Laser scanner function blocks for PSENscan, motion monitoring for AGVS

From software version 11.3.0, new blocks provide for the most secure und flexible monitoring of the:

  • Laser scanner PSENscan:

The zone selection function block enables productive solutions for stationary and mobile danger zone safeguarding in conjunction with the safety laser scanner PSENscan, used to monitor 2D zones. In this way, for example, it is possible to monitor open robot cells safely, or also guarantee efficient processes in a logistics or production environment.

  • Automated guided vehicle systems (AGVS):
  • Motion monitoring software blocks for safe synchronisation monitoring, for example, plus three others for safe position monitoring (Safe Position Comparison, Safe Position Range and Safe Position Monitoring), are available for monitoring automated guided vehicle systems (AGVS). They are used in conjunction with the safe motion monitoring modules PNOZmulti 2.
  • With safe synchronisation monitoring, two axes are compared – a comparison is possible based on higher, lower or same speed. Tolerance windows can be defined in the software tool, enabling an even more flexible application. PNOZ m EF 2MM is the module of choice in this regard. Safe detection of anomalies in the synchronisation of two axes protects human and machine. Also, synchronous operation can be monitored on synchronous axes. Safe path detection is enabled by monitoring and comparing the two drive axes on an AGVS.
  • When safe position monitoring is used, the position and position range of an axis can be monitored. The modules PNOZ m EF 1MM/2MM/1MM 2DO can be used for this purpose. The steering axis and current position of an axis can be monitored safely once a reference marker to detect the zero point has been set.

Hardware – Perfectly tailored to the application:

  • The input module PNOZ m ES 16DI has 16 digital inputs and monitors standard applications.
  • The communication module PNOZ m EF EtherCAT FSoE enables safe data transfer with Safety over EtherCAT in conjunction with the base unit PNOZ m B1. PNOZmulti 2 can be used as FSoE Master, FSoE Slave or EtherCAT Slave.
  • Decentralised input and output modules PDP67 F 10DI4DO (VA) forward signals from the connected sensors to the safe small controller PNOZmulti 2. New features are the four safe semiconductor outputs on the PDP67, which enable safe sensor technology such as the modular safety gate system PSENmlock to be connected directly to the PNOZmulti 2 via cable. Up to four of the modules with protection type IP67 can be connected to the PNOZmulti 2 via the link module PNOZ m EF PDP-Link. Up to four safe sensors per PDP67 module - a total of up to 64 sensors - can be monitored flexibly in the field in this way. A version with stainless steel screw connections is available, for use in the food industry for example. M12 plug-in connectors link sensors and actuators quickly and easily to the PDP67 module. Complicated wiring is avoided. That reduces costs when expanding and commissioning modular production plants.

Your application advantages:

  • Maximum flexibility due to the module program configuration
  • Safe solutions for stationary and mobile danger zone safeguarding with the laser scanner PSENscan
  • Parameters for motion monitoring safety functions are easily set via software, for the safe monitoring of automated guided vehicle systems (AGVS)
  • Software tool can be used free of licensing costs

Software PNOZmulti Configurator – What’s new in Version 11.2

These are the new features you'll find in Version 11.2.0:

  • Key-in-pocket solution:

For maintenance safeguarding and to protect against unauthorised restart, combine the small controllers PNOZmulti 2 and reader units PITreader with RFID technology. Three new function elements in the software tool enable you to implement safe access and restart management for plant and machinery. All keys that are logged in are stored in a list in the user program. A machine is not enabled to restart until all keys are signed out. Manipulation is excluded, as the key is not permitted to remain in the PITreader, either when accessing or leaving the plant. The blind spot element requires areas of the plant that are not in view to be inspected prior to any restart. In this way you can provide flexible safeguarding of service operations on your plant and machinery. You can sign in and out at any door and thus save time, particularly on larger plants.

  • Standalone base unit PNOZ m C0 with security key:

The planned new Machinery Regulation (successor to the Machinery Directive) requires security mechanisms that prevent access to device data. Security features are already accounted for in the PNOZ m C0. So PNOZmulti 2 is well equipped for the future.

  • Monitoring analogue values safely:

Two new function elements are available for the safe analogue input module PNOZ m EF 4AI, when configuring the module program. The differentiation element detects a change of the analogue value over a certain period. The “ramp” element is used if you wish to monitor whether a value moves within defined upper and lower limits. If a value exceeds or falls below these limits – plus a tolerance – PNOZmulti 2 initiates appropriate remedial measures. Whether you are monitoring fill level, temperature, pressure, speed or other values - your processes are safe.

  • Up to 84 standard outputs on the base unit PNOZ m B1:

You can connect up to 6 output modules PNOZ m ES 14 DO to the base unit PNOZ m B1. So you can activate indicator lights, signal lamps, illuminated pushbuttons and many other standard tasks, economically.

Software tool Version 10.14, long-term-supported version

  • Contains hardware from the product ranges PNOZmulti Classic and PNOZmulti Mini
  • This version can be used to migrate PNOZmulti Classic or Mini* projects to PNOZmulti 2
  • PNOZmulti Classic/Mini projects, open, edit projects
  • Existing licence keys can be used

Download now! Version 10.14 PNOZmulti Configurator

*The product ranges PNOZmulti Classic and PNOZmulti Mini were discontinued as of 31.12.2024.

More information about the discontinuation

Top
Pilz Österreich

Pilz Ges.m.b.H. Sichere Automation
Wagramer Straße 19
1220 Wien
Österreich

Telephone: +43 1 7986263-0
E-Mail: [email protected]

Technischer Support

Telephone: +43 1 7986263-444
E-Mail: [email protected]

Open contact form
Telephone:+43 1 7986263-0
Mail: [email protected]

What can we do for you?


I understand that, unless I give my consent, any personal data collected will only be used for processing orders and dealing with my enquiries. Further information on data protection and contact details for our data protection officer are available here: Pilz data protection
Consent can be withdrawn at any time (E-Mail will suffice).

* Mandatory field