Safe direction (SDI)

Monitoring the Safe Direction (SDI) in accordance with EN 61800-5-2 prevents the motor from moving in an invalid direction. If a deviation is detected in the direction of movement, the defined reaction is performed.

Safe monitoring of the direction of movement is used frequently in combination with the safely limited speed (SLS). Here too, the drive-integrated solution enables the fastest possible shutdown. In practice, this combination makes sense in particular when work is performed in the danger zone and it must be ensured that a drive moves in the required direction and at a defined maximum speed.

The safety function is also fulfilled by the speed monitor PNOZ s30!

SDI – Safe direction
Top
Pilz Österreich

Pilz Ges.m.b.H. Sichere Automation
Wagramer Straße 19
1220 Wien
Österreich

Telephone: +43 1 7986263-0
E-Mail: [email protected]

Technischer Support

Telephone: +43 1 7986263-444
E-Mail: [email protected]

Was this article helpful?
Open contact form
Telephone:+43 1 7986263-0
Mail: [email protected]

What can we do for you?


I understand that, unless I give my consent, any personal data collected will only be used for processing orders and dealing with my enquiries. Further information on data protection and contact details for our data protection officer are available here: Pilz data protection
Consent can be withdrawn at any time (E-Mail will suffice).

* Mandatory field