CANopen

CANopen is a communications protocol that is mainly used in automation technology and for networking within vehicles and complex devices. The communications protocol is based on the serial bus system CAN (Controller Area Network), which was developed in the early 1980s. Both CAN and CANopen are international standards.


Structure

The subscribers are generally connected to the CANopen network via 5-pin open style connectors, 5-pin M12 or 9-pin Sub-D connectors. A maximum of 127 subscribers can be connected in a CANopen network. The communication speed can be set in defined increments in the range from 10 kbit/s to 1 Mbit/s. The length of the CANopen network depends on the communication speed.


The following product groups have a CANopen interface:

Decentralised I/O system PSSuniversal - Communication modules

Configurable safety system PNOZmulti - Communication modules

Configurable small control system PNOZmulti Mini - Communication modules

Configurable control system PNOZmulti 2 - Communication module

Control systems PSSuniversal PLC and PSSuniversal multi - Gateways

Control system PMCprimo

Top
Pilz Österreich

Pilz Ges.m.b.H. Sichere Automation
Wagramer Straße 19
1220 Wien
Österreich

Telephone: +43 1 7986263-0
E-Mail: [email protected]

Technischer Support

Telephone: +43 1 7986263-444
E-Mail: [email protected]

Was this article helpful?
Open contact form
Telephone:+43 1 7986263-0
Mail: [email protected]

What can we do for you?


I understand that, unless I give my consent, any personal data collected will only be used for processing orders and dealing with my enquiries. Further information on data protection and contact details for our data protection officer are available here: Pilz data protection
Consent can be withdrawn at any time (E-Mail will suffice).

* Mandatory field