Laws and standards in Europe

Europe

Various directives apply within the European Union; these must be incorporated into domestic law by the individual member states.

One common feature of many directives is mandatory CE marking for products that fall under the scope of these directives.

Non-EU countries sometimes have differing laws and directives.

Relationship between directives, laws and standards in Europe

The directives are addressed to EU member states, who are obliged to incorporate the European directives into domestic law. In Germany, for example, this is incorporated via the Product Safety Act (ProdSG).

Standards are not legally binding and merely represent the state of science and technology at the time of publication. Standards may not be applied in an EU conformity assessment procedure until they are harmonised with an EU directive through publication in the Official Journal of the European Communities. Satisfying the requirements leads to "presumption of conformity". This presumption of conformity says that a manufacturer can assume that when the standard is implemented correctly, the essential health and safety requirements of the EU directive defined in the standard's Annex are met.

If a manufacturer applies European directives and the relevant harmonised standards correctly, then in product liability terms, the burden of proof is reversed. This means that, in the event of an accident or fatality, the market surveillance authorities (in Germany the factory inspectorate) or the public prosecutor's office must prove to the manufacturer that directives and harmonised standards have not been considered and implemented correctly.

EU countries

Machinery Directive

When the Machinery Directive (MD) was ratified in 1993, the aim was to remove trade barriers and enable a free internal market within Europe. After a two-year transition period, the Machinery Directive has been binding in Europe since 01.01.1995. It describes standardised health and safety requirements for interaction between human and machine and replaces the host of individual state regulations that existed on machinery safety. The Machinery Directive 2006/42/EC has applied since 29.12.2009.

Mandatory CE marking

There is mandatory CE marking for products that fall under the scope of one or more of the directives below. These products must also be accompanied by a declaration of conformity.

With a declaration of conformity, which is legally binding, manufacturers confirm that their product meets all the requirements of the European directives relating to their product. This means they can launch and sell their product within the scope of the EU, currently 27 EU states including Switzerland, Norway and Turkey, without consideration of any national provisions.

Declarations of conformity for Pilz products are available in our download area.

Examples of EU directives with mandatory CE marking

Great Britain

Great Britain left the EU on 31.12.2020. Britain’s exit from the European Union has significant effects for plant and machine manufacturers. We’ll explain what these are:

Further information

However, existing regulations will remain in force!

In Great Britain, specific use of work equipment regulations apply: Provision and Use of Work Equipment Regulations (PUWER).

These regulations cover all work equipment used by staff in the course of their work - from a hammer to mechanical presses and motor vehicles. The "use" of work equipment also covers maintenance, cleaning, transportation or commissioning of the work equipment.

PUWER not only requires appropriate work equipment to be provided and correctly maintained, but also that risks resulting from use of the work equipment must be prevented in advance.

Great Britain

What is PUWER?

The "Provision and Use of Work Equipment Regulations" (PUWER) were created within the scope of the "Health and Safety at Work etc. Act 1974" (HSW Act) and came into force on 5 December 1998. The main objective of PUWER is to guarantee the provision of safe work equipment over the whole service life, irrespective of its state, age or origin.

Who is responsible?

Each employer is obliged to assess the risks to the health and safety of people in their workplace. The regulations not only require that employers provide appropriate, safe work equipment and machinery, but also that they consider the work conditions and risks for the health and safety of staff, including the provision of appropriate training.

What does PUWER cover?

PUWER applies for the provision and use of all work equipment and machinery, including mobile equipment and hoists - in short, everything from a tool to a standalone machine or assembly plant.

Further information:

Pilz Österreich

Pilz Ges.m.b.H. Sichere Automation
Modecenterstraße 14
1030 Wien
Österreich

Telephone: +43 1 7986263-0
E-Mail: pilz@pilz.at

Technischer Support

Telephone: +43 1 7986263-444
E-Mail: techsupport@pilz.at

Was this article helpful?