Austria | english

CE marking

The control cabinet and machine have different numbers on the CE mark. Is this permitted?

Control cabinets are often certified in accordance with the Low Voltage / EMC Directive, particularly if the control cabinet comes from another manufacturer. So it is both possible and permitted for the machine and control cabinet to have difference CE marks.


Pilz Austria

Pilz Ges.m.b.H. Safe Automation
Modecenterstraße 14
1030 Wien

Telephone: +43 1 7986263-0

Technical Support

Telephone: +43 1 7986263-444