Ostfildern, 23 Sept 2025

Pilz at Hydrogen Technology World Expo in Hamburg, Hall 5, Stand: H20 - Automation for the H2 future – safe, smart, scalable

Whether it's for production via electrolysis, refuelling or combustion, Pilz offers tailor-made solutions for the hydrogen industry. The automation expert will present its comprehensive range at Hydrogen World Expo in Hamburg from 21 to 23 October 2025. Experts from Pilz will also provide insights into the norms and standards that are important for the development and integration of hydrogen technologies.

Hydrogen production requires the very highest safety standards. At Hydrogen World Expo, Pilz will use an electrolyser model to demonstrate how the small controller PNOZmulti 2 and the automation system PSS 4000 reliably safeguard processes in alkaline or PEM electrolysis. Among other things, the safety controllers monitor sensors for gas and flame detection and automatically initiate measures such as valve venting in the case of danger – in compliance with the international standard ISO 22734. Visitors to the stand will also gain practical insights into how access regulations for electrolysis plants can be implemented safely. 

Failsafe control at hydrogen refuelling stations
Permanent view of pressure and temperature monitoring, as well as filling and emptying speeds: the safe small controller PNOZmulti 2 from Pilz offers reliable analogue value processing for transfer processes at hydrogen refuelling stations. Pilz experts on the stand will explain how pressure ramp monitoring can be used to safely control changeable process variables and detect any anomalies or errors at an early stage. The “Safe ramp monitoring” block integrated in the software tool PNOZmulti Configurator keeps a reliable eye on the limit parameters for pressure monitoring. Thanks to safety-related accuracy of 1 per cent, a PNOZmulti 2 analogue input guarantees precise limit value setting with dynamic limit value monitoring up to safety level SIL 3 in accordance with IEC 62061. Also, the automation system PSS 4000 is already proven when it comes to maintaining an overview of all the safety functions on hydrogen refuelling stations – on the cooling system and high-pressure storage tanks, and when dispensing hydrogen.

Burning hydrogen – but safely!
Pilz offers certified burner controllers as well as comprehensive services such as risk assessments for furnaces that are being converted to hydrogen operation or are already “H2 ready”. Implementation is in accordance with the standards ISO 13577 and PAS 4445:2025. The focus is on safe monitoring of invisible flames, leakages and the gas control section. Experts from Pilz will be available at the exhibition to advise visitors on burner management systems.

Pilz at Hydrogen Technology World Expo 2025: Hall 5, Stand: H20

Industry-proven solutions from Pilz enable the safe monitoring and control of processes across the whole hydrogen added value chain. Experts from Pilz will provide information at Hydrogen Expo Europe. (Photo: © Pilz GmbH & Co. KG)
Industry-proven solutions from Pilz enable the safe monitoring and control of processes across the whole hydrogen added value chain. Experts from Pilz will provide information at Hydrogen World Expo. (Photo: © Pilz GmbH & Co. KG)

Industry-proven solutions from Pilz enable the safe monitoring and control of processes across the whole hydrogen added value chain. Experts from Pilz will provide information at Hydrogen World Expo. (Photo: © Pilz GmbH & Co. KG)

Top
Pilz Österreich

Pilz Ges.m.b.H. Sichere Automation
Wagramer Straße 19
1220 Wien
Österreich

Telephone: +43 1 7986263-0
E-Mail: [email protected]

Pressekontakt

Telephone: +43 1 7986263-56
E-Mail: [email protected]

Open contact form
Telephone:+43 1 7986263-0
Mail: [email protected]

What can we do for you?


I understand that, unless I give my consent, any personal data collected will only be used for processing orders and dealing with my enquiries. Further information on data protection and contact details for our data protection officer are available here: Pilz data protection
Consent can be withdrawn at any time (E-Mail will suffice).

* Mandatory field