Ostfildern, 22 Jul 2025

Indian approval for the PLC-based Failsafe Network Multiplexer from Deltron and Pilz - One platform for all signalling tasks

In future, the Failsafe Network Multiplexer (FNmux) from the Indian signalling technology manufacturer Deltron will be able to control automatic line blocks in India. The SIL 4 platform solution, based on the safe, modular railway control system PSSrail from the automation expert Pilz monitors interlockings, level crossings and signals. FNmux now has the necessary railway approval and is making a decisive contribution to the digitisation of the Indian railway infrastructure.

FNmux is the result of a long-term collaboration between Deltron and the automation expert Pilz. In March, FNmux was officially approved by the Indian supervisory authority "Research Design and Standards Organisation" (RDSO).

A safe package
The SIL 4-capable signalling solution FNmux combines safety and control intelligence to monitor level crossings, interlockings and signals in automatic line blocks in a particularly cost-effective manner. The multiplex method is used, i.e. several signals are transferred simultaneously via optical fibre. FNmux thus enables technology openness, which is a crucial requirement in the rapidly growing Indian infrastructure. The innovation lies in the solution's modularity: via the inputs and outputs of the railway control system PSSrail, the solution can be adapted flexibly to a variety of applications in the extensive Indian Railways network, and is easily configured. With its real-time response, redundancy and reliability, PSSrail offers additional strengths when used at Deltron.

Future-proof railway control system
With this jointly developed solution, Deltron and Pilz are laying an important foundation for the digitisation of India's railway infrastructure. FNmux can be connected to other components across a range of manufacturers and is therefore equipped for digitisation tasks.

The SIL 4 platform solution FNmux from Deltron is based on the safe, modular railway control system PSSrail from Pilz and monitors interlockings, level crossings and signals. (Photo: © Pilz GmbH & Co. KG)
The SIL 4 platform solution FNmux from Deltron is based on the safe, modular railway control system PSSrail from Pilz and monitors interlockings, level crossings and signals. (Photo: © Pilz GmbH & Co. KG)

The SIL 4 platform solution FNmux from Deltron is based on the safe, modular railway control system PSSrail from Pilz and monitors interlockings, level crossings and signals. (Photo: © Pilz GmbH & Co. KG)

Top
Pilz Österreich

Pilz Ges.m.b.H. Sichere Automation
Wagramer Straße 19
1220 Wien
Österreich

Telephone: +43 1 7986263-0
E-Mail: [email protected]

Pressekontakt

Telephone: +43 1 7986263-56
E-Mail: [email protected]

Open contact form
Telephone:+43 1 7986263-0
Mail: [email protected]

What can we do for you?


I understand that, unless I give my consent, any personal data collected will only be used for processing orders and dealing with my enquiries. Further information on data protection and contact details for our data protection officer are available here: Pilz data protection
Consent can be withdrawn at any time (E-Mail will suffice).

* Mandatory field