22 Jan 2026

Confident about audits and compliance: always inspection-ready with the MYZEL Lifecycle Platform

New regulations, such as the EU Machinery Regulation, increase evidence and auditability requirements. Companies maintain an overview with the MYZEL Lifecycle Platform, because MYZEL digitally maps your operation, machinery and personnel.

Why is digital documentation becoming mandatory?

From January 2027, the EU Machinery Regulation will apply directly in all member states. It mandates digital documentation, clear cybersecurity requirements and stricter procedures for machinery with increased risk. So companies must guarantee that all documents are up to date and consistent. This applies to internal audits as well as external inspections by customers or authorities.

Man despairing over paperwork

Auditability as a competitive factor?

Today, audits are a strategic issue. They influence handovers, acceptance and credibility with partners. When evidence is scattered, the effort required for preparation and follow-up work increases considerably. If compliance data is managed centrally, it creates transparency for deadlines, responsibilities and status. As a result, organisational burdens such as fines or costs due to production downtimes are reduced and your company’s reliability and image are enhanced.

How does MYZEL maintain order?

Each system, down to the smallest component, is linked to relevant documents such as declarations of conformity, test reports and safety validations. Employees are recorded with evidence of their qualifications and permissions. The dashboard means that those responsible see immediately where action is required. With MYZEL you maintain an overview, because all data is stored securely in one central location. Digital artifacts ensure the integrity of the data. Once created, they cannot be changed and they can be audited.

 

In MYZEL you are supported by digital workflows:

  • mySafeDesign
  • mySafeOperation
  • myAccessControl

These workflows are digital process sequences, which create a structure for risk assessments, maintenance and inspection records, as well as management of access rights.

More about workflows

Structure MyCore Workflows Dashboard

Your data is secure in MYZEL:

All templates are up to date and are based on applicable standards. The cloud-based platform meets the highest security standards with ISO/IEC 27017 and ISO/IEC 27018; data is stored exclusively in the EU. All this helps to ensure that your compliance and audit documentation is designed securely, transparently and clearly, enabling you to meet all your obligations without a care.

Do you want to be inspection-ready at all times during everyday production?

Whether it’s internal audit rounds or external certifications:

With MYZEL, all evidence is stored centrally on one platform. You can immediately verify which tests have been carried out, which qualifications are valid, and which safety measures have been documented. This creates trust and reduces the effort required for preparation and follow-up work.

Auditor speaking with those responsible, tablet in hand
Top
Pilz Österreich

Pilz Ges.m.b.H. Sichere Automation
Wagramer Straße 19
1220 Wien
Österreich

Telephone: +43 1 7986263-0
E-Mail: [email protected]

Was this article helpful?
Open contact form
Telephone:+43 1 7986263-0
Mail: [email protected]

What can we do for you?


I understand that, unless I give my consent, any personal data collected will only be used for processing orders and dealing with my enquiries. Further information on data protection and contact details for our data protection officer are available here: Pilz data protection
Consent can be withdrawn at any time (E-Mail will suffice).

* Mandatory field