Закрыть
Pilz International
Пожалуйста, выберите страну
Выберите свою страну, чтобы получить доступ к предназначенным для нее материалам
Вы искали «PNOZ msi11p adapter cable 1»
Вы имели в виду: PNOZ msi1ap adapter cable 1.5m?
Temporary licence for the software PSS WIN-PRO for use of the full
version on one workstation. Includes a licence key for activating the
full functionality over a period of four months. Note: Does not
include software! CD must be ordered separately, if required.
по запросу
Upgrade licence for updating the version number of an present project
licence for the full version of the PSS WIN-PRO software. Includes a
licence key for activating the full functionality. Note: Does not
include software! CD must be ordered separately, if required.
по запросу
Upgrade licence for updating the version number of an present user
licence for the full version of the PSS WIN-PRO software. Includes a
licence key for activating the full functionality. Note: Does not
include software! CD must be ordered separately, if required.
по запросу
User licence for the PSS WIN-PRO software for use of the full version
on an additional workstation. Includes a licence key for activating
the full functionality. Only valid for expanding a basic licence. Note:
Does not include software! CD must be ordered separately, if required.
по запросу
Basic licence for the PSS WIN-PRO software for use of the full version
on one workstation. Includes a licence key for activating the full
functionality. Note: Does not include software! CD must be ordered
separately, if required.
по запросу
Multi-User licence for the PSS WIN-PRO software for for use of the
full version on several workstations. Includes a licence key for
activating the full functionality. Note: Does not include software! CD
must be ordered separately, if required.
по запросу
User licence for the PSS WIN-PRO software for use of the service
version on an additional workstation. Includes a licence key for
activating the full service functionality. Only valid for expanding a
basic licence. Note: Does not include software! CD must be ordered
separately, if required.
по запросу
Upgrade licence for updating the version number of an existing project
licence for the service version of the PSS WIN-PRO software. Includes
a licence key for activating the service functionality. Note: Does not
include software! CD must be ordered separately, if required.
по запросу
Basic licence for the PSS WIN-PRO software for use of the service
version on one workstation. Includes a licence key for activating the
service functionality. Note: Does not include software! CD must be
ordered separately, if required.
по запросу
Temporary licence for the software PSS WIN-PRO for use of the service
version on a workstation. Includes a licence key for activating the
service functionality for a period of two months Note: Does not
include software! CD must be ordered separately, if required.
по запросу
Temporary licence for the software PSS WIN-PRO for use of the service
version on a workstation. Includes a licence key for activating the
service functionality for a period of four months Note: Does not
include software! CD must be ordered separately, if required.
по запросу
Upgrade licence for updating the version number of an existing basic
licence for the service version of the PSS WIN-PRO software. Includes
a licence key for activating the service functionality. Note: Does not
include software! CD must be ordered separately, if required.
по запросу
Temporary licence for the software PSS WIN-PRO for use of the service
version on a workstation. Includes a licence key for activating the
service functionality for a period of three months Note: Does not
include software! CD must be ordered separately, if required.
по запросу
Multi-User licence for the PSS WIN-PRO software for using the service
version on several workstations. Includes a licence key for activating
the service functionality. Note: Does not include software! CD must be
ordered separately, if required.
по запросу
Upgrade licence for updating the version number of an existing
Multi-User licence for the service version of the PSS WIN-PRO software.
Includes a licence key for activating the service functionality. Note:
Does not include software! CD must be ordered separately, if required.
по запросу
Upgrade licence for updating the version number of an existing user
licence for the service version of the PSS WIN-PRO software. Includes
a licence key for activating the service functionality. Note: Does not
include software! CD must be ordered separately, if required.
по запросу
Зашифрованная USB-память в прочном металлическом корпусе. Длябезопасного
и
удобного хранения и передачи единиц PAS. В комплект входитфлэш-
накопитель
USB 3.1 промышленного качества на 16 ГБ.
по запросу
PMI v707e
Статья о поэтапном выводе из эксплуатации
PMIvisu, диагностический рабочий терминал, 7", разрешение 800 x 600
пикселей, емкостный сенсорный экран, TFT, ОЗУ 512 МБ, флэш-память 2 ГБ,
1 портRJ45 на 100 МБит/с, 1 основной порт USB 2.0, часы реального
времени с подпиткой отконденсатора, 24 В пост. тока, 6 Вт,
экономичная версия, ОС Linux, установленная cистема PASvisu Runtime
слицензией, предустановленное ПО: ПО визуализации Pilz.
Важная информация: Данный элемент находится в конце жизненного цикла Важная информация: Данный элемент находится в конце жизненного цикла продукта и, свяжитесь с вашим представителем PILZ, чтобы найти подходящую альтернативу или продукт-замену.
по запросу
PMI v704e
Статья о поэтапном выводе из эксплуатации
PMIvisu, диагностический рабочий терминал, 4,3", разрешение 480 x 272
пикселей, емкостный сенсорный экран, TFT, ОЗУ 512 МБ, флэш-память 2 ГБ,
1 портRJ45 на 100 МБит/с, 1 основной порт USB 2.0, часы реального
времени с подпиткой отконденсатора, 24 В пост. тока, 4 Вт,
экономичная версия, ОС Linux, установленная система PASvisu Runtime
слицензией, предустановленное ПО: ПО визуализации Pilz.
Важная информация: Данный элемент находится в конце жизненного цикла Важная информация: Данный элемент находится в конце жизненного цикла продукта и, свяжитесь с вашим представителем PILZ, чтобы найти подходящую альтернативу или продукт-замену.
по запросу
PMI v815
Статья о поэтапном выводе из эксплуатации
PMIvisu, диагностический рабочий терминал, 15,6", разрешение 1920 x 1080
пикселей, емкостный сенсорный экран, TFT, ОЗУ 4 ГБ, SSD 32 ГБ, 2 порта
RJ45 на 1 ГБит/с, 1 основной порт USB 3.0, 2 основных порта USB 2.0, 1
порт HDMI,1 порт VGA, часы реального времени с подпиткой от
конденсатора, 12 ... 30 В пост.тока, 38,5 Вт, ОС Windows 10 IOT,
установленная система PASvisu Runtime с лицензией,предустановленное
ПО: PMI Assistant v8, сервер и клиент PASvisu, PVIS OPC Server
UA, прошивка PSS 4000 (сервер OPC UA).
Важная информация: Данный элемент находится в конце жизненного цикла Важная информация: Данный элемент находится в конце жизненного цикла продукта и, свяжитесь с вашим представителем PILZ, чтобы найти подходящую альтернативу или продукт-замену.
по запросу
Следующие продукты были добавлены в Вашу Корзину
Сохранить корзину
Создать новый заказ или оформить индивидуальное ценовое предложение.