Compare 0
Video tutorials
Global Site | english
You have now of 6 products to compare

Rotary encoder PSENenco

Standard rotary encoder – but safe

Rotary encoder PSENenco

The rotary encoders PSENenco are used to determine position and speed. The rotary encoder available in the first expansion phase is an absolute encoder, which is used in the automation system PSS 4000. It supplies diverse, absolute position values, which are verified in the software block. The sensor has a magnetic and an optical measuring system. You get two devices in one!

Safe position and safe speed – The benefits

  • Safe evaluation of speed and position
  • The safe monitoring function is transferred to the user software
  • High flexibility when monitoring limit values due to dynamic limit value monitoring in the user program
  • Mechanical rotary cam arrangement is replaced by the safe electronic rotary cam arrangement PSS 4000 (incl. rotary encoder PSENenco)
Safe position and safe speed – The benefits

Features of the rotary encoder

Features of the rotary encoder
  • Two encoders in one housing
  • Diverse, 2-channel (1 x optical, 1 x magnetic)
  • 2 SSI interfaces
  • SIL CL 3 and PL e in the automation system PSS 4000

Application of rotary encoder PSENenco

The rotary encoders PSENenco are used above all in the area of mechanical presses. The "safe electronic rotary cam arrangement" solution completely replaces conventional mechanical rotary cam arrangements. The combination of the rotary encoder PSENenco with the control system PSSuniversal PLC and the corresponding software blocks achieves SIL 3. Other application areas of the rotary encoder are wherever safe position detection is necessary.

Application of rotary encoder PSENenco

Industry uses of the rotary encoder

Our product range: Rotary encoder PSENenco

PSENenco rotary encoder

PSENenco is a standard rotary encoder. SIL 3 and PL e are achieved in combination with the control system PSSuniversal PLC and the corresponding software blocks.

Download

Please wait while data is being loaded

Please wait while data is being loaded

Headoffice

Pilz GmbH & Co. KG
Felix-Wankel-Straße 2
73760 Ostfildern
Germany

Telephone: +49 711 3409-0
E-Mail: pilz.gmbh@pilz.de

Technical Support

Telephone: +49 711 3409 444
E-Mail: support@pilz.com

Americas

  • United States (toll-free): +1 877-PILZUSA (745-9872)
  • Canada: +1 888-315-PILZ (315-7459)
  • Brazil: + 55 11 4942-7028
  • Mexico: +52 55 5572 1300

Europe

  • Ireland: +353 21 4804983
  • United Kingdom: +44 1536 462203
  • Italy: +39 0362 1826711
  • France (toll-free): +33 3 88104000
  • Belgium: +32 9 321 75 70
  • Russia: +7 495 6654993
  • Switzerland: +41 62 88979 32
  • Netherlands: +31 347 320477
  • Austria: +43 1 7986263-444
  • Denmark: +45 74436332
  • Finland: +358 10 3224030 / +45 74436332
  • Spain: +34 938497433
  • Germany: +49 711 3409 444
  • Turkey: +90 216 5775552
  • Sweden: +46 300 13990 / +45 74436332

Asia Pacific

  • China: +86 21 60880878-216
  • Japan: +81 45 471 2281
  • South Korea: +82 31 778 3390
  • Australia: +61 3 9560 0621
  • Taiwan: +886 2 25700068
  • New Zealand: +64 9 6345350