When man and robot work together ...

Mar 5, 2012

Take a look at the product animation for SafetyEYE – the world's first safe camera system.

All optoelectronic protective devices provide barrier-free safety. But only the camera system SafetyEYE is able to monitor warning and detection zones safely in 3D. Particularly in production processes where man and machine work actively together on a workstation, a high level of safety is required. SafetyEYE enables safe co-operation between man and robot. By showing warning and detection zones, the worker is prevented from approaching the danger zone while the robot arm is in motion.

See for yourself in our SafetyEye Animation!


Further benefits of SafetyEYE at a glance:

  • High productivity, thanks in particular to ergonomic workstations and efficient work practices
  • Excellent manipulation protection
  • Rapid installation and simple commissioning using just a few components
  • Simple configuration software
  • User-friendly diagnostics


Further information:

If you have any questions please contact our technical support.