Feb 7, 2024

Safe small controller PNOZmulti 2 – up and down without a care!

Lifts are still among the safest means of transport. To date, their safety-related functions are primarily implemented through mechanical-electrical components. So in addition to floor switches, limit switches and inspection switches, most lifts have a separate shaft copying system and speed limitation device. To date, only in isolated cases are electronic components equipped with safety functions.

Programmable electronic systems, such as the configurable safe small controller PNOZmulti 2, are what are called PESSRAL (Programmable Electronic Systems in Safety-Related Applications for Lifts). They combine these functions, so replacing mechanical components that are high maintenance and susceptible to ageing.

Safety components for lifts and goods lifts may only be sold in Europe if they have previously been certified by an independent, notified body. This is regulated by the European Union in the Lifts Directive 2014/33/EU.

Two mechanics working on a lift
Employees from PILZ and TÜV Süd at the handover of the certification document

Pictured are: Mark Dietz from TÜV Süd; Jürgen Kitzing, Andreas Volland and Stephan Rauch from Pilz, Carina Rebernak from TÜV Süd

Type examination certificate awarded for use in elevators, lifts, escalators

The base units of the PNOZmulti 2 product range and associated expansion modules have been certified by TÜV SÜD as a programmable electronic system, known as PESSRAL, in accordance with the directive 2014/33/EU. TÜV Süd presented Pilz with the certification document at the world’s leading international trade fair Interlift, in Augsburg in October 2023.

These standards were the basis for inspection:

  • EN 81-20:2020
  • EN 81-22:2021
  • EN 81-50:2020
  • EN 115-1:2017

Very large range of applications possible

That’s how users and manufacturers reach their destination safely with the safe small controllers PNOZmulti 2 – whether that’s to the top of the summit or deep underground – the multi-talented PNOZmulti is everywhere:

  • Goods lifts
  • Passenger lifts
  • Domestic lifts
  • Lifting platforms
  • Vehicle/car lifts
  • Stage lifts
  • Ship lifts
  • Residential lifts
  • Patient lifts
  • Disabled lifts
  • Dumb waiters
  • Service lifts
  • Escalators
  • Moving walkways
  • Travelators
  • Conveyor belts
Three empty escalators in a building
Contact

Pilz Automation Safety L.P.
7150 Commerce Boulevard
Canton, MI 48187
USA

Telephone: +1 734 354-0272
E-Mail: info@pilzusa.com

Was this article helpful?