The technical solution of the fully synchronized seventh axis for Stäubli's robotic arms was created thanks to intensive cooperation between PILZ, Stäubli and FeiCut in Czechia
Aug 4, 2023
Fully synchronized 7th axis for Stäubli robots
It is a fully synchronous seventh axis controlled via a Stäubli CS9 PLC. This means that with the robotic arm you don't just travel from place to place, but while maintaining high precision, you can, for example, machine a workpiece along its entire length without interrupting the machining process.
This is a significant extension of reach, when the robotic arm is placed on a modular track that can reach a length of several tens of meters.
The PILZ company is a major subcontractor of the inverter and servomotor, which are key to this solution. The supplier of the entire solution is primarily the company FeiCut, but you can also purchase individual parts of the system together with the robot from Stäubli.
Our PMC SC6 servo amplifiers are used in the application: https://www.pilz.com/cs-CZ/products/drive-technology/servo-amplifiers/pmcmodulo
And our PMC EZ servo motors: https://www.pilz.com/cs-CZ/products/drive-technology/motors/pmc-ez
Currently, the demo application is available in the application room of the Stäubli company in the city Pardubice in Czechia.
Contact to the responsible person from the company PILZ:
Ing. Patrik Predný, email: [email protected] , tel.: +420 603 225 376
Contact to the responsible person from the company FeiCut:
Ing. Martin Kaván, [email protected], tel.: +420 724 704 948
Direct link to more detailed information about the track here
Contact person responsible at Stäubli:
Mr. Jan Koplík, [email protected], tel. +420 734 254 977
General information about Stäubli robotics here
Please, do not hesitate to contact us.
Plně synchronizovanou 7. osu jsme prezentovali na Technology Days, které proběhlo 6. - 8 .6. 2023 v Pardubicích.
Zde se můžete podívat na krátké video našeho stánku kde jsme prezentovali naše řešení 7. plně synchronní osy:
Pilz Slovakia s.r.o.
Ludvíka Svobodu 2674/1
058 01 Poprad
Slovakia
Telephone: +421 52 772 8201
E-Mail: [email protected]
Telephone: +49 711 3409 - 0
E-Mail: [email protected]