Economical solutions for safe automation – including comprehensive services: This is Pilz’s focus at the regional exhibitions for industrial automation, “all about automation”, in Hamburg (29 and 30 June 2022) and Chemnitz (28 and 29 September 2022). The automation expert will be showing modular safety gate systems, which satisfy the demands of both safety and security. Live at the event, visitors can test how easy it is these days to create individual safety solutions using the myPNOZ Configurator.
Ostfildern, 7 Jun 2022
Pilz at “all about automation” 2022 in Hamburg and Chemnitz - Experience individual safety, live!
Pilz will be showing the various options and types of safety gate guarding, live on site. Visitors to the exhibition will see all the versatile components for safety gate monitoring and access control in action: This includes not only the mechanical safety gate system PSENmech with guard locking, but also the PSENmlock door handle module for safe interlocking and guard locking up to the highest category PL e, with integrated optional escape release, which is especially suited for more complex applications.
Added to this is the operating unit PITgatebox with new, preconfigured versions with combinations of pushbuttons, key switches and emergency stop pushbuttons for simple operation of safety gate systems. Together with the integrated new reader unit PITmode fusion, Pilz offers an economical solution for safe control of access to plant and machinery, as well as safe operating mode selection. The solution thus covers the requirements for safety & security. With the configurable safe small controller PNOZmulti 2, Pilz is also introducing a future-proof solution for implementing numerous safety functions with maximum flexibility.
Safety in batch size 1
In addition to safety gate guarding, the new type of modular safety relay myPNOZ will also be on display. It can be assembled individually via the online tool myPNOZ Creator. myPNOZ monitors the following safety functions: E-STOP, safety gate, light curtain, two-hand IIIA/C and enabling switches. The safety relay is delivered pre-assembled, set and tested and so is a completely individualised system, ready to install. The logic operations for the safety functions are pre-defined via the plug-in sequence, so no programming knowledge is required. Visitors to the exhibition stand can test the myPNOZ Creator at the shows and create their safety solution live.
Safety & security talk
Anyone wanting to discover more about tailor-made safety is invited to the presentation “With myPNOZ to tailor-made safety” at the exhibition in Hamburg, in the thematic block “Safety”. Our experts will explain the new type of continuous digital process that encompasses creation, simulation, ordering and commissioning in the myPNOZ Creator.
In Chemnitz, experts from Pilz invite visitors to a deep exchange of knowledge as part of the presentation “Safety gate solutions – the safe way!”, where they will discuss new solutions for monitoring, guard locking and operating safety gates, in the thematic block “Safety & Security”. Both presentation series are available to all visitors free of charge.
Further information on the exhibition stand is available at:
Hamburg, Messe Hamburg-Schnelsen, 29 + 30 June 2022, Stand EG-300
Chemnitz, Messe Chemnitz, 28 + 29 September 2022, Stand 441
Pilz GmbH & Co. KG
Felix-Wankel-Straße 2
73760 Ostfildern
Germany
Telephone: +49 711 3409-0
E-Mail: pilz.gmbh@pilz.de
Telephone: 0711 / 3409 - 158
E-Mail: publicrelations@pilz.com