The modular safety relay myPNOZ would not be called "modular" if it couldn't easily be embedded in your application. We explain exactly how that works in our FAQs about the new product.
14-Dec-2021
The new safety relay myPNOZ
With myPNOZ you have on one hand the flexibility to exchange individual modules even after commissioning. On the other hand you also have the possibility to choose the right combination from 12 different expansion modules as well as semiconductor and relay outputs. LED indicators directly on the device take care of any fault detection.
- Can I transfer data from the myPNOZ Creator into Eplan?
Yes, that's very easy to do. An XML file of the configuration can be created in the myPNOZ Creator and exported. In turn this file can be imported into the EPLAN Data Portal – the result quite simply is a complete system macro, which makes it easier for you to create the circuit diagram.
- What rules apply for myPNOZ when commissioning?
Plug-and-play: when you receive myPNOZ it is preset and can be commissioned straight away. The modules are connected via BUS connector and the system's voltage supply comes via the head module, so there is no need for wiring between the modules. That saves a lot of time during commissioning.
- What are my diagnostic options with the myPNOZ?
Each myPNOZ module has LEDs for every function, for the inputs and outputs as well as for reset. A higher level error display can also be used for precision diagnostics, identifying which module may have a fault. The faulty module can then be exchanged individually on the plant, without having to dismantle the system.
Pilz lndia Pvt Ltd
5th Floor, Aston Plaza, Katraj - Ambegaon Road, Ambegaon BK,
Pune - 411046
India
Telephone: +91 20 69501100
E-Mail: info@pilz.in