Jämför 0
Instruktionsvideor
Sverige | svenska
Du jämför nu av 6 produkter

Beroende på behoven kan du välja mellan olika licenser med stigande antal funktioner. Välj mellan baslicens, användarlicens, projektlicens, basuppgraderingslicens, användaruppgraderingslicens eller projektuppgraderingslicens.

Produktnr. beskrivning
301288B

Basic licence for the PSS WIN-PRO software for use of the full version on one workstation. Includes a licence key for activating the full functionality. Note: Does not include software! CD must be ordered separately, if required.

301288K

User licence for the PSS WIN-PRO software for use of the full version on an additional workstation. Includes a licence key for activating the full functionality. Only valid for expanding a basic licence. Note: Does not include software! CD must be ordered separately, if required.

301288U

Upgrade licence for updating the version number of an present basic licence for the full version of the PSS WIN-PRO software. Includes a licence key for activating the full functionality. Note: Does not include software! CD must be ordered separately, if required.

301289B

Basic licence for the PSS WIN-PRO software for use of the service version on one workstation. Includes a licence key for activating the service functionality. Note: Does not include software! CD must be ordered separately, if required.

301289K

User licence for the PSS WIN-PRO software for use of the service version on an additional workstation. Includes a licence key for activating the full service functionality. Only valid for expanding a basic licence. Note: Does not include software! CD must be ordered separately, if required.

301289U

Upgrade licence for updating the version number of an existing basic licence for the service version of the PSS WIN-PRO software. Includes a licence key for activating the service functionality. Note: Does not include software! CD must be ordered separately, if required.

301290G

 

301290K

 

Nedladdning

Vänta medan data läses in

Vänta medan data läses in