Ostfildern, 21 Mar 2024

New operation element PIT oe ETH with activatable Ethernet port can be used for Security - Secure and flexible operation

Pilz adds the operation element PIT oe ETH to its portfolio of control and signal devices. PIT oe ETH has an activatable Ethernet port, thus protecting freely accessible industrial Ethernet interfaces from improper access. As such the compact operation element provides greater Security. As an industrial Ethernet interface it can act like a firewall, not only protecting network connections from unauthorised access externally, but also from direct access to human machine interfaces and control data internally.

On plant and machinery, PIT oe ETH protects the network, and therefore know-how and investment. The new activatable and de-activatable Ethernet interface gives users the opportunity to protect their network fully: it is possible to control and trace individually and securely who has access to sensitive machine data when, and how. Production security is increased as a result.

Active/activated operation protection guards against improper access
Because in combination with the reader unit PITreader from Pilz, the Ethernet interface can only be activated with the relevant permission. In other words, only authorised persons have permission to use these interfaces temporarily. To create new configurations, programs or backup copies, for example. Thanks to 24 V standard inputs, also available with 5 V, they are flexible and can be activated via any control output. This enables users to have full data flow control over their networks.

Meets all normative specifications 
The new operation element PIT oe ETH meets the safety requirements of machine manufacturers and operators alike: The Machinery Regulation is making security measures mandatory for machine manufacturers from January 2027 at the latest.
For machine operators in Germany, the technical rules for operational safety TRBS 1115 already apply as an extension to the Ordinance on Industrial Safety and Health, which requires unnecessary hardware interfaces to be deactivated or blocked, and unauthorised communication connections to be shut down. So PIT oe ETH helps with the implementation of the legal and normative specifications, which ultimately protects investment and minimises costs.

Installation made simple
The compact operation elements are intended for 22.5 mm diameter mounting cutouts in accordance with EN 60947-5-1, with anti-rotation protection. As a result, they fit seamlessly into the plant and machine design.
The operation elements PIT oe 4S and PIT oe USB from the PIToe product range are also available to users: with the operation element PIT oe 4S, digital inputs and outputs can be switched and displayed, the operating mode for example. PIT oe USB has an activatable USB interface for plant and machinery, enabling programs to be imported without manipulation, for example. 
As such the compact operation elements have advantages when it comes to installing or retrofitting them into consoles, control panels or command panels. In conjunction with the access permission system PITreader, both provide secure assess management.
 

The new operation element PIT oe ETH from Pilz, with activatable Ethernet port, protects network connections from unauthorised access both internally and externally, like a firewall. PIT oe ETH expands the Pilz portfolio of control and signal devices. (Photo: © Pilz GmbH & Co. KG)
The new operation element PIT oe ETH from Pilz, with activatable Ethernet port, protects network connections from unauthorised access both internally and externally, like a firewall. PIT oe ETH expands the Pilz portfolio of control and signal devices. (Photo: © Pilz GmbH & Co. KG)

The new operation element PIT oe ETH from Pilz, with activatable Ethernet port, protects network connections from unauthorised access both internally and externally, like a firewall. PIT oe ETH expands the Pilz portfolio of control and signal devices. (Photo: © Pilz GmbH & Co. KG)

Top
Headoffice

Pilz GmbH & Co. KG
Felix-Wankel-Straße 2
73760 Ostfildern
Germany

Telephone: +49 711 3409-0
E-Mail: [email protected]

Corporate and Technical Press

Telephone: +49 711 3409 - 0
E-Mail: [email protected]

Open contact form
Telephone:+49 711 3409-0
Mail: [email protected]

What can we do for you?


I understand that, unless I give my consent, any personal data collected will only be used for processing orders and dealing with my enquiries. Further information on data protection and contact details for our data protection officer are available here: Pilz data protection
Consent can be withdrawn at any time (E-Mail will suffice).

* Mandatory field