The new standard is currently being developed internationally as ISO 20607. It specifies basic requirements for the design of instruction handbooks for machinery. Safety components are also affected because the new standard will be harmonised with the Machinery Directive. The current version of the new standard can already be used as a stable basis for development work in engineering. It will probably be published in the course of 2019!
May 28, 2019
What is the present status of the new DIN EN ISO 20607?
What is the relationship with the Machinery Directive?
Annex ZA to the draft standard defines the relationship with the Machinery Directive MD 2006/42/EC. So the standard is a guideline when creating instruction handbooks for machinery.
prEN ISO 20607 deals with the safety-related content, the corresponding structure and presentation of the instruction handbook, taking into account all phases of the life cycle of the machine. The standard establishes the principles which are indispensable to provide information on residual risks.
As soon as DIN EN ISO 20607 is published in the Official Journal of the EU there is presumption of conformity with the Machinery Directive 2006/42/EC and the standard will be included in the list of harmonised standards. It is not clear yet whether there will be a transition period. If so, this may be a maximum of three years. A significantly shorter transition period is also possible.
What is the significance of DIN EN ISO 20607 for engineering?
Manufacturers of machinery and safety components will need to deal with the potential consequences and repercussions on existing and future instruction handbooks at an early stage. Non-compliance with the standard may mean that there is no CE conformity for machinery and safety components!
As soon as the standard is published it will be available to purchase via the ISO web store.
Pilz GmbH & Co. KG
Felix-Wankel-Straße 2
73760 Ostfildern
Germany
Telephone: +49 711 3409-0
E-Mail: pilz.gmbh@pilz.de
Americas
- Mexico: +52 55 5572 1300
- Brazil: + 55 11 4942-7032
- United States (toll-free): +1 877-PILZUSA (745-9872)
- Canada: +1 888-315-PILZ (315-7459)
Europe
- Ireland: +353 21 4804983
- Austria: +43 1 7986263-444
- Finland: +358 10 3224030 / +45 74436332
- Italy: +39 0362 1826711
- Russia: +7 495 6654993
- Spain: +34 938497433
- Denmark: +45 74436332
- Switzerland: +41 62 889 79 32
- Germany: +49 711 3409 444
- Belgium: +32 9 321 75 70
- Turkey: +90 216 5775552
- Netherlands: +31 347 320477
- France (toll-free): +33 3 88104000
- Sweden: +46 300 13990 / +45 74436332
- Portugal: +351 229 407 594
- United Kingdom: +44 1536 460866
Asia Pacific
- South Korea: +82 31 778 3390
- New Zealand: +64 9 6345350
- Japan: +81 45 471 2281
- Taiwan: +886 2 25700068
- Singapore: +65 6829 2920
- Thailand: +66 210 54613
- China: +86 400-088-3566
- Australia (toll-free): +61 3 9560 0621 / 1300 723 334