1 Jan 1970

Helping exporters to comply with local regulations


A machine that is fully compliant with standards and regulations in one country may not conform to national rules in another. Machine exporters are therefore faced with complex issues relating to regulatory compliance, as are users when they move machinery from one country to another. Ensuring compliance in a cost-effective and timely manner is critical to such companies.

Fortunately Pilz, with its global network of subsidiaries, has the expertise and resources to provide appropriate support services. In partnership with the client company's engineering team, Pilz consultants conduct the required assessments and plan the necessary strategies to ensure compliance with the appropriate ISO, IEC, ANSI and/or other standards, as well as interpreting CE marking requirements if appropriate.

The Pilz consultants and engineers will also ensure that the appropriate documentation is in place at the right time so as to avoid project delays. This includes taking responsibility for the technical files and, where necessary, submitting them to the regulatory authorities.

Taking full advantage of the global network of Pilz subsidiaries, Pilz safety experts provide client companies with first-hand, local interpretation of the standards and regulations in force in the country in which the machine will be used.

Please contact Pilz to request more information about International Compliance Services.