1 Jan 1970

PNOZmulti Configurator v5.3 supports analogue inputs

Pilz is releasing a new version of the drag-and-drop Configurator for the PNOZmulti modular safety controller. This incorporates a number of improvements and enhancements over the previous version, 5.2.2, the most important of which is support for the PNOZ ma1p analogue input module that was announced recently.

The new version of the Configurator enables users to create safety-related control systems that incorporate a maximum of four PNOZ ma1p modules per PNOZmulti base unit, with each analogue module accepting two analogue inputs. Depending on the configuration of the hardware and safety logic, the analogue modules meet the requirements of EN IEC 62061 SIL2 or SIL3, as well as performance level (PL) e of EN ISO 13849-1.

A wide range of sensors with +/-10V or 0-20mA signals can be used - typically in a dual redundant configuration - such as encoders, temperature sensors, pressure sensors or position/level sensors. The PNOZmulti controller can then monitor four range limits or a maximum of eight threshold levels per input. Reaction time is just 75ms.

Status is indicated via LEDs on the front of the analogue input module and, if installed, via the PVIS 'intelligent diagnostics' system and a suitable Pilz display. In addition, the actual analogue values can be transmitted to other devices via a PNOZmulti fieldbus module.

Compared with the traditional technique of using a separate unit to set a level on an analogue signal (for example, by means of an analogue-to-digital converter), the PNOZmulti analogue functionality offers greater simplicity, a lower risk of errors, and a reduced requirement for engineering time - which together are likely to result in cost savings.

Support for the PNOZ ma1p analogue module is the main benefit of the latest release of the Configurator, but users also gain from an improved menu structure and navigation, as well as better print options.

Customers running a previous version of the Configurator with a licence less than 12 months old are entitled to free upgrades to version 5.3; for those with licences older than this there is a small charge of £122.40.

Please contact Pilz to request more information about PNOZmulti Configurator software licences.