Safety-related equipment

Is it permitted for the machine and control cabinet on a plant to each have a CE mark?

As control cabinets are often built externally, they are provided with a CE mark in accordance with the Low Voltage and EMC Directive. CE marking for a machine is conducted in accordance with the Machinery Directive. As such it is permitted for the control cabinet and machine to have a separate CE mark.

 

Contact

Pilz Automation Safety Canada L.P.
6695 Millcreek Drive, Unit 8
Mississauga, ON, L5N 5R8
Canada

Telephone: +1 905 821 7459
E-Mail: info@pilz.ca

Technical Support

Telephone: +1 888-315-PILZ (315-7459)
E-Mail: tech@pilz.ca

Was this article helpful?