How is the quality of Pilz ROS packages guaranteed?

The high-quality Pilz ROS packages are designed for use in an industrial environment. The source code is in line with Pilz's rigorous standards as well as ROS-Industrial development standards and is regularly tested by means of unit, integration and acceptance tests. The test results are available on the Pilz GitHub page; they can be reproduced there using test logs (Travis processes).

ROS modules

Contact

Pilz Automation Safety Canada L.P.
6695 Millcreek Drive, Unit 8
Mississauga, ON, L5N 5R8
Canada

Telephone: +1 905 821 7459
E-Mail: info@pilz.ca

Technical Support

Telephone: +1 888-315-PILZ (315-7459)
E-Mail: tech@pilz.ca

Was this article helpful?