Firmware Update PSS 4000 head unit

Example: Firmware update from FW-Version 1.5.0 to 1.6.0. The steps for firmware update are identical for all firmware versions.

How to Update the Firmware of PSS 4000 head modules

  • Check if a SD card is inside the PSS 4000 device
  • Make a direct connection from your PC to the PLC-head-module or I/O-head-module
  • Change the IP from your PC in the range from the devices (for example PC:169.254.1.5 and PSS:169.254.1.1).
  • Switch on the PSS 4000 Head
  • Start PAS4000
  • Click on the “Open Online Network Editor”-Button
  • Click the Button “Scan network”
  • Now you see your device. If you see flashing lights in the line of your PSS 4000 Head. You have a correct connection. Only then a Firmware Update is possible.
  • Load the firmware zip file for the PSSu Head Module
  • Therefore take the mouse und click with the right button on your device.
  • Choose “Load Firmware File”
  • Choose the right firmware file for your PSSu Head Module (Example: PSSu_H_PLC1_FS_SN_SD-1_6_0)
  • Click on "Open".
  • The firmware package file has been loaded.
  • Click on “OK” to continue.
  • Start the firmware update.
  • Therefore take the mouse und click with the right button on your device.
  • Choose “Update firmware”.
  • Confirm with „yes“.
  • Firmware update is starting.
  • Firmware update was successful.

Downloads

Contact

Pilz Automation Safety Canada L.P.
6695 Millcreek Drive, Unit 8
Mississauga, ON, L5N 5R8
Canada

Telephone: +1 905 821 7459
E-Mail: info@pilz.ca

Technical Support

Telephone: +1 888-315-PILZ (315-7459)
E-Mail: tech@pilz.ca

Was this article helpful?