Sensor technology

Light beam devices PSENopt

What is the difference between a BCM and ACM configuration?

  • In BCM mode you have the option to use the buttons and the LED interface (transmitter/receiver) to select basic functions/parameters.
  • In ACM mode you have the option to use the PC software PSENopt Configurator (only for the receiver) to select advanced functions/parameters. The PSEN op Advanced Programming Adapter is required for configuration via software.

 

Contact

Pilz Automation Safety Canada L.P.
6695 Millcreek Drive, Unit 8
Mississauga, ON, L5N 5R8
Canada

Telephone: +1 905 821 7459
E-Mail: info@pilz.ca

Technical Support

Telephone: +1 888-315-PILZ (315-7459)
E-Mail: tech@pilz.ca

Was this article helpful?