Video tutorials for the automation system PSS 4000: Establishing communication interface connections via Ethernet and fieldbuses

Ethernet

What Ethernet communication interfaces are available in the automation system PSS 4000?
How can Ethernet communication interfaces be configured in PAS4000?

Fieldbuses

What fieldbus communication interfaces are available in the automation system PSS 4000?
How can fieldbus connections be configured in PAS4000?

The automation system PSS 4000 now offers a device interface for communication with ProfiNETProfinet networks.

Contact

Pilz Automation Safety Canada L.P.
6695 Millcreek Drive, Unit 8
Mississauga, ON, L5N 5R8
Canada

Telephone: +1 905 821 7459
E-Mail: info@pilz.ca

Technical Support

Telephone: +1 888-315-PILZ (315-7459)
E-Mail: tech@pilz.ca

Was this article helpful?