Standards are documented, generally voluntary agreements which establish the criteria for products, services and procedures. Standards can be used to guarantee that products and services are fit for purpose, comparable and compatible.
Standards are documented, generally voluntary agreements which establish the criteria for products, services and procedures. Standards can be used to guarantee that products and services are fit for purpose, comparable and compatible.
The EN standards are applied at European level. They are normally developed at the initiative of the EU by the European standards organisations CEN and CENELEC. (CEN and CENELEC build the framework for all the national standards organisations in Europe.) CEN and CENELEC also divide out the standards (CENELEC: Electrical and electronic engineering. CEN: Mechanics). Today, many standards are developed almost in a package as an IEC or ISO standard in co-operation with the EU via CEN and CENELEC. EN IEC or EN ISO standards are the result of these efforts. Standards in Europe are subdivided into what are termed A, B and C standards.
Pilz Belgium cvba
Poortakkerstraat 37/0201
9051 Gent (Sint-Denijs-Westrem)
Belgium
Telephone: +32 9 3217570
E-Mail: info@pilz.be
Poortakkerstraat 37/0201
Gent (Sint-Denijs-Westrem)
Belgium
Telephone: +32 9 321 75 70
E-Mail: info@pilz.be
Telephone: +32 (0)9 321 75 70
E-Mail: techsupport@pilz.be